Skip to main content
randyao12345
Associate III
Dec 5, 2014 2:03 AM UTC
Question

Interrupt problem and UART problem

Posted on December 05, 2014 at 03:03

Hi ST forum,

I have two separate problems: 1. How do I configure an interrupt to do X on rising edge and Y on falling edge? Currently, I can only do rising edge: (Solved, see below)

/*********************************************************************************************************

 

** Function name:           EXTI_PA0_Config

 

** Descriptions:            Configures interrupt for PA0

 

** Parameters: None

 

*********************************************************************************************************/

 

 

 

void EXTI_PA0_Config(void)

 

{

 

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA,ENABLE);

 

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

 

 

 

GPIO_main.GPIO_Mode = GPIO_Mode_IN;

 

GPIO_main.GPIO_Speed = GPIO_Speed_25MHz;

 

GPIO_main.GPIO_PuPd = GPIO_PuPd_NOPULL;

 

GPIO_main.GPIO_Pin = GPIO_Pin_0; //Output PA0

 

GPIO_Init(GPIOA,&GPIO_main);

 

 

 

EXTI_main.EXTI_Line = EXTI_Line0;

 

EXTI_main.EXTI_Mode = EXTI_Mode_Interrupt;

 

EXTI_main.EXTI_Trigger = EXTI_Trigger_Rising; //need raising falling

 

EXTI_main.EXTI_LineCmd = ENABLE;

 

EXTI_Init(&EXTI_main);

 

 

 

SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);

 

 

 

NVIC_main.NVIC_IRQChannel = EXTI0_IRQn; //connect EXTI to line 0

 

NVIC_main.NVIC_IRQChannelPreemptionPriority = 0x01;  //set both preemptive priority and sub-priority to lowest

 

NVIC_main.NVIC_IRQChannelSubPriority = 0x01;

 

NVIC_main.NVIC_IRQChannelCmd = ENABLE;

 

NVIC_Init(&NVIC_main);

 

}

 

 

 

void EXTI0_IRQHandler(void){

 

    NVIC_ClearPendingIRQ(EXTI0_IRQn);

 

 

 

    if(flag==0)

 

    {

 

    flag=1;

 

    }

 

    else if(flag==1)

 

    {

 

    flag=0;

 

    }

 

    EXTI->PR|=(1<<0); //write 1 to PR to clear - write 1 at bit 0?

 

}

 

Problem 2: I want to be able to receive UART. Currently I can only transmit UART. (Partially solved with bugs, see below)

/*********************************************************************************************************

 

** Function name:           UART1_Init

 

** Descriptions:            Initializes UART2_TX at PA2

 

** Parameters: None

 

*********************************************************************************************************/

 

 

 

void UART1_Init(void)

 

{

 

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

 

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

 

 

 

    GPIO_main.GPIO_Pin = GPIO_Pin_2;

 

GPIO_main.GPIO_Mode = GPIO_Mode_AF;

 

GPIO_main.GPIO_PuPd = GPIO_PuPd_UP;

 

GPIO_main.GPIO_Speed = GPIO_Speed_50MHz;

 

GPIO_main.GPIO_OType = GPIO_OType_PP;

 

GPIO_Init(GPIOA, &GPIO_main);

 

 

 

GPIO_PinAFConfig(GPIOA,GPIO_PinSource2,GPIO_AF_USART2);

 

 

 

USART_main.USART_Mode = USART_Mode_Tx; //Transmit Mode, Receiver mode not currently required

 

USART_main.USART_BaudRate = 115200; //This is right

 

USART_main.USART_WordLength = USART_WordLength_8b; //8 bit data transmit

 

USART_main.USART_Parity = USART_Parity_No; //

 

USART_main.USART_StopBits = USART_StopBits_1; // 1 stop bit

 

USART_main.USART_HardwareFlowControl =     USART_HardwareFlowControl_None;

 

USART_Init(USART2,&USART_main);

 

        USART_Cmd(USART2,ENABLE);

 

}
    This topic has been closed for replies.

    3 replies

    randyao12345
    Associate III
    Dec 12, 2014 6:10 PM UTC
    Posted on December 12, 2014 at 19:10

    I got the interrupt problem solved by doing this (after entering interrupt, check for port level).

    void EXTI9_5_IRQHandler(void)

     

    {

     

    if (EXTI_GetITStatus(EXTI_Line5) != RESET) //Filter line 5

     

    {

     

       EXTI_ClearITPendingBit(EXTI_Line5);

     

       if(GPIO_ReadInputDataBit(GPIOB,GPIO_Pin_5))

     

       {

     

        GPIOD->BSRRL = GPIO_Pin_12; //test and debug only

     

        flag = 1;

     

       }

     

       else if(!GPIO_ReadInputDataBit(GPIOB,GPIO_Pin_5))

     

       {

     

        GPIOD->BSRRH = GPIO_Pin_12; //test and debug only

     

        flag = 0;

     

       }

     

    //    UART1_Send(Message_StopMotor,5);

     

    }

     

    }

     

    For the UART, I'm stuck on this problem: I'm doing a loopback test, but valid data only displays 3500 baud or below. Over 4000 it displays some nonsense..

     

     

    Here's my codes:

    void UART1_Init(void)

    {

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);

        RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA,ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG,ENABLE);

        GPIO_main.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;

    GPIO_main.GPIO_Mode = GPIO_Mode_AF;

    // GPIO_main.GPIO_PuPd = GPIO_PuPd_UP;

    GPIO_main.GPIO_Speed = GPIO_Speed_50MHz;

    // GPIO_main.GPIO_OType = GPIO_OType_PP;

    GPIO_Init(GPIOA, &GPIO_main);

    GPIO_PinAFConfig(GPIOA,GPIO_PinSource9,GPIO_AF_USART1);

    GPIO_PinAFConfig(GPIOA,GPIO_PinSource10,GPIO_AF_USART1);

    USART_main.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; //Transmit Mode, Receiver mode not currently required

    USART_main.USART_BaudRate = 3500; //Current baud rate 115200 bit/s

    USART_main.USART_WordLength = USART_WordLength_8b; //8 bit data transmit

    USART_main.USART_Parity = USART_Parity_No; //No parity bits

    USART_main.USART_StopBits = USART_StopBits_1; // 1 stop bit

    USART_main.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    // USART_Init(USART1,&USART_main);

    //  USART_Cmd(USART1,ENABLE);

        USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); //enables

    USART_Init(USART1,&USART_main);

    USART_Cmd(USART1, ENABLE);

        NVIC_main.NVIC_IRQChannel = USART1_IRQn;        // we want to configure the USART1 interrupts

        NVIC_main.NVIC_IRQChannelPreemptionPriority = 0;         // this sets the priority group of the USART1 interrupts

        NVIC_main.NVIC_IRQChannelSubPriority = 0; // this sets the subpriority inside the group

        NVIC_main.NVIC_IRQChannelCmd = ENABLE; // the USART1 interrupts are globally enabled

    NVIC_Init(&NVIC_main);        // the properties are passed to the NVIC_Init function which takes care of the low level stuff

    }

    void USART1_IRQHandler(void)

    {

    if (USART_GetITStatus(USART1, USART_IT_RXNE) != RESET)

    {

    // USART_ClearITPendingBit(USART1, USART_IT_RXNE);

    // rx[rx_index] = USART_ReceiveData(USART1);

    rx[rx_index] = USART1->DR;

    if(rx_index>9)

    {

    rx_index = 0;

    }

    rx_index++;

    }

    }

    in main:

    int main(void)

    {

    LED_Init(); //Initializes LED outputs

    UART1_Init(); //Initializes UART1 at PA9

    EXTI_PB5_Config(); //Configures interrupt for PB5

    int k = 0;

    UART1_Send(Message_SetSpeed,7);

        while(1)

        {

        for(k=0;k<rx_index;k++)

        {

        printf(''\n%d: %X'',k,rx[k]);

        }

        }

    }

    (Set speed was defined as: uint8_t Message_SetSpeed[6] = {0x01,0xA1,0x9C,0x40,0x82,0x04}; //Speed set at 4000RPM)

    Tesla DeLorean
    Guru
    Dec 12, 2014 8:21 PM UTC
    Posted on December 12, 2014 at 21:21

    What board are you doing this on? The STM32F4-DISCO has a huge bulk capacitor hung off the USART1 pins, which is going to limit it's rate/usability.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    randyao12345
    Associate III
    Dec 12, 2014 9:25 PM UTC
    Posted on December 12, 2014 at 22:25

    I am using the discovery board. Maybe that is the problem? Thus switching to USART2/3 would solve the problem?