Skip to main content
obogush
Associate
June 9, 2009
Question

Interrupt priority grouping field, NVIC_PriorityGroup

  • June 9, 2009
  • 4 replies
  • 1017 views
Posted on June 09, 2009 at 08:24

Interrupt priority grouping field, NVIC_PriorityGroup

    This topic has been closed for replies.

    4 replies

    obogush
    obogushAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Hi,

    The description and number of NVIC_PriorityGroup constants in the firmware library does not match the PRIGROUP field description in the Cortexâ„¢-M3 Technical Reference Manual.

    Is there a bug?

    Thanks,

    Olek

    artur2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Hi,

    At least for me it was a little confusing that ST naming (in that matter) is opposite to ''official'' ARM naming.

    I mean that ST names priority group using number of bits assigned for preempt priority field and ARM uses names coming from exact value of PRIGROUP.

    ST:

    NVIC_PriorityGroup_0 - 0 bits for pre-emption priority 4 bits for subpriority, defined value of PRIGROUP 7

    ARM:

    PRIGROUP 7 - 0.8 indicates no pre-emption priority, eight bits of subpriority

    Descriptions match but their names not.

    Regards,

    obogush
    obogushAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear STOne-32,

    Thank you very much for your clarification. It is exactly what I was looking for. The UM0306 manual actually states that there are 16 programmable priority levels. However, it does not mention that only values from 7 to 3 are accepted by the PRIGROUP field in the Application Interrupt and Reset Control Register due to this limitation.

    Thank you again.

    Best regards,

    Olek

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear olek ,

    Could you give more details what do you mean by does not match ?

    The Cortexâ„¢-M3 Technical Reference Manual is a generic document from ARM implementing up to 241 external Interrupts in the micro & up to 8-bits of priorities.

    In STM32F10x we have 43 external interrupts (different from the Cortex-M3 core) and only 16 levels (4-bit) of priorities are implemented. Which is enough to handle all the Interrupts priorities levels.

    Implementing all bits is a waisting of the silicon area. ;)

    Regards,

    STOne-32.