Question
Interrupt Issues
Posted on May 23, 2018 at 13:49
I have a CubeMX generated project using the STM32L I have TIM2 configured for IC and OC. I am using the Cube generated ISR callbacks for the TIM and SYSTICK. The SYSTICK callback works fine by itself and the TIM_IC_Capture callback works fine. What I am seeing is that when I make a call toHAL_TIM_OnePulse_Start_IT(&htim2, TIM_CHANNEL_1) that my SYSTICK callback no longer seems to run. Could this be an interrupt priority issue? Ideas? Thanks!
void SystemClock_Config(void)
{
...
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
static void MX_NVIC_Init(void)
{
/* EXTI4_15_IRQn interrupt configuration */
HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);
/* TIM2_IRQn interrupt configuration */
HAL_NVIC_SetPriority(TIM2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM2_IRQn);
}
void HAL_SYSTICK_Callback(void)
{
ServiceTimers();
}�?�?�?�?
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
ServiceHeater();
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
#isr-systick