Skip to main content
Associate III
Feb 4, 2025 7:26 AM UTC
Solved

Internal Pull up STM32G4 series

Hello,

I am using the internal pull up for the input pins, but when read the port status using the program, it always reads 0 instead of 1. I expected it to read 1 and if make that pin grounded it shall read 0. 

 

 

This topic has been closed for replies.
Hl_stBest answer
ST Employee
Feb 4, 2025 9:25 AM UTC

I couldn´t see anything wrong in your code. I tried to do some easy example and it works right and pin input value is also seen in debugger. Do you have connected anything externally to MCU pins? 

 

 

int main(void)
{
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* Configure the system clock */
 SystemClock_Config();

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 /* USER CODE BEGIN 2 */
 /* USER CODE END 2 */

 /* Infinite loop */
 while (1)
 {
 HAL_GPIO_WritePin(USER_LED_GPIO_Port, USER_LED_Pin, 
 HAL_GPIO_ReadPin(INPUT_PULL_UP_GPIO_Port, INPUT_PULL_UP_Pin));
 }
}

static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(USER_LED_GPIO_Port, USER_LED_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : INPUT_PULL_UP_Pin */
 GPIO_InitStruct.Pin = INPUT_PULL_UP_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(INPUT_PULL_UP_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : USER_LED_Pin */
 GPIO_InitStruct.Pin = USER_LED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(USER_LED_GPIO_Port, &GPIO_InitStruct);
}

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

12 replies

ST Employee
Feb 4, 2025 8:01 AM UTC

Hello,

can you also share complete configuration of these pins?

Thank you

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STUser34Author
Associate III
Feb 4, 2025 8:34 AM UTC

This is the code

#define ON 1

static void MX_GPIO_Init(void)
{
	GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /* USER CODE BEGIN */

 /*Configure GPIO pin Output Level */
 // HAL_GPIO_WritePin(GPIOB, GPIO_PIN_11, GPIO_PIN_RESET);

 /*Configure GPIO pin : PB11 */
 GPIO_InitStruct.Pin = GPIO_PIN_11;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_15;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : PC6 PC7 PC8 */
 GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pins : PA8 PA9 PA10 */
 GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 /* USER CODE END */
}
MC_VehicleMode_Status_t SetVehicleMode(MCI_Handle_t *pHandle)
{
 uint8_t l_portb_pin11_state_u8=0;
 uint8_t l_portb_pin12_state_u8=0;
 uint8_t l_porta_pin8_state_u8=0;
 uint8_t l_portc_pin7_state_u8 = 0;
 uint8_t l_portb_pin15_state_u8 = 0;
 uint8_t l_porta_pin9_state_u8 = 0;

 l_portb_pin11_state_u8 = HAL_GPIO_ReadPin(GPIOB,GPIO_PIN_11);
 l_portb_pin12_state_u8 = HAL_GPIO_ReadPin(GPIOB,GPIO_PIN_12);
 
 if(l_portb_pin11_state_u8 == ON)
 {
 pHandle->VehicleMode = MCM_REVERSE_MODE;
 }
 else if(l_portb_pin12_state_u8 == ON)
 {
 pHandle->VehicleMode = MCM_CITY_MODE;
 }
}

But in the code when i debug it always reads as 0 instead of 1. I have added only the main section of the code. Please let me know if anything else to be shared or added.

 

Ozone
Principal
Feb 4, 2025 9:03 AM UTC

I suppose the values are consistent with the input register values of the GPIO in the debugger.

Have you tried a, say, 5k external pull-up resistor ?
And have you physically measured the voltage on the respective pins ?