Question
Internal Oscillator Clock issue - STM32U375VGT6Q
- 5 replies
- 360 views
We are using MPN: STM32U375VGT6Q in one of our projects, with the internal RC oscillator configured as the core clock source.
During board validation, when the system clock was configured to the maximum frequency of 96 MHz, we observed a signal integrity issue. Specifically, the SPI clock signal (96 MHz / 2) does not return properly to the 0V base level,
To rule out any PCB trace-related effects, we measured the signal directly at the MCU pin.as attached.
Please help us with the necessary resolution for the issue observed.