Internal FLASH and timer1
In my STM32L496 MCU I saw that if I activate timer1(PWM channel1) is not possible to use internal flash because FLASH_SR_PGSERR go up just after initialization (Hal_Init).
while, if I disable the timer (in cube) and regenerate code, flash works as expected.
So my question is: is it a problem to use timer1 and flash together?
Thanks in advance