Skip to main content
Associate III
Sep 30, 2026 1:01 PM UTC
Question

Interfacing with 1.8V OctoSPI RAM

Hello everyone,

I am designing a board using an STM32U5 / STM32H5 microcontroller and I have a question regarding the power supply architecture, specifically concerning the independent voltage domains.

My Scenario:

  • Main VDD: 3.3V (required for correct USB functionality/transceiver management via VDDUSB).
  • VDDIO2: 1.8V (supplied independently to interface with low-voltage external peripherals).

The Issue:
According to the reference manuals and datasheets, there are specific power-up and power-down sequencing requirements, as well as constraints on the voltage levels between different domains (e.g., VDDIOx vs VDD).

Is it fully supported to run VDD / VDDUSB at 3.3V while simultaneously running an OCTOSPI/HyperBus at 1.8V?

Thanks in advance for your help!

2 replies

mƎALLEm
ST Technical Moderator
Sep 30, 2026 1:19 PM UTC

Hello ​@Fin95 ,

Your request will be escalated to OLS.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Sep 30, 2026 1:24 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.