Skip to main content
vishal patel
Associate II
Feb 25, 2017 10:44 AM UTC
Solved

Interfacing STM32 with External 512kx16 SRAM, 8bit data only accessible per one address of RAM

Posted on February 25, 2017 at 11:44

Hi,I have STM32F4 interfaced with the external SRAM sized 512kx16 array. Now what I believe is (Pls correct me if i am wrong), Pointing to Every incremental Address should give me 16bit data. because SRAM is interfaced with 16bit wide data bus (non multiplexed)

For Example: 0x64000000 is the base address of my external SRAM. And I want to write hello, to this RAM, then It should happen like...

on 0x64000000 location, data should be written, 'H' 'E' &

on 0x64000001 location, data should be written, 'L' 'L' &

on 0x64000002 location, data should be written, 'O' 0xff .

And the same is should be getting in read back.

But What actually occurs is

on 0x64000000 location, data iswritten, 'H' 'E' &

on 0x64000001 location, data is written, 'E' 'L' &

on 0x64000002 location, data

is

written, 'L' 'L' &

on 0x64000003 location, data is written, 'L' 'O' &

on 0x64000004 location, data is written, 'O' 0xff .

So If I want to get the write data, I will have to read back 16 bit data from location

0x64000000,0x64000002, and 0x64000

Can Anyone Has the experience of interfacing 512kx16bit array SRAM ? and facing the similar issues ??

#external-ram #sram #stm32 #dma #fsmc

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This topic has been closed for replies.
T J
T JBest answer
Senior III
Feb 28, 2017 6:31 AM UTC
Posted on February 28, 2017 at 06:31

yes, I can see your diagram looks good.

and the problem is that pins A0-A18 are actually shifted inside the processor to A1-A19 (suggested by Clive)

So you can be sure your addressing is now 20 bits wide,

So the result is that your address range should be 0- 0xFFFFF

please try that,

15 replies

T J
Senior III
Feb 25, 2017 3:16 PM UTC
Posted on February 25, 2017 at 16:16

The SRAM/SDRAM/FLASH all have a unique address for each Byte...

it is a byte addressing scheme...

Usually you would declare as:

//align (2);             // this is done by default for int16_t

int16_t Variable1;

char array(7);      // 1 byte remains unused

int16_t Variable2;

Tesla DeLorean
Guru
Feb 25, 2017 3:28 PM UTC
Posted on February 25, 2017 at 16:28

How do you suppose you can write 'H' and 'E' into the same byte?

You'd need to treat the memory the same regardless of how it is physically bused. 16-bit wide means you can write two bytes at ones, but they still consume two bytes, so the stride would be two to the next pair

ie

Write 'H' together with 'E' to 0x64000000

Write 'L' together with 'L' to 0x64000002

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
world04
Visitor II
Feb 26, 2017 3:04 PM UTC
Posted on February 26, 2017 at 16:04

The Bus connection and the access of them by the CPU kernal are independed and unknown by the programming language. In every case, you need to take care about the alignment of your declared variables or structures, if you wanna do a direct register or memory access.  How wide the bus is and how many clock cycles the mpu needs to do, is hidden by the program. The memory storage is byte-wide organized. As an example - a charcter like ' ' is coded by ASCII in 0x20 or dec 32 and could be coded by just 7 bit's - does the MPU wrote just 7 bit's into the memory to store them, or store it 8 bit's? 

if a value is 32 Bit's wide, the clock cylces that the mpu need's to store this 4 byte wide value depended on the used databus bit's of the memeory who are connected to the MPU. In every case, you need to declare the used

databus bit's in the  FSMC definition, before you can use them and how fast this is possible. The fastest way to get or store data is of course a 32 bit connectivity for data. The thumb command set of the ARM is traditionaly just 16bit wide.

 
vishal patel
Associate II
Feb 27, 2017 6:51 AM UTC
Posted on February 27, 2017 at 07:51

Thanks all For Replies,

I am using AS6C8016, which is 512kx16bit array SRAM. It has A0-A18 Address bus, so technically I can address only 524287 location, lets say 512K, And now according to you, If I can access 1 byte only per one location, then How can I access 1 MByte memory, [which is as per their data sheet, 8,388,608-bit/8MBit/1Mbyte].

It has UB/LB control pins too, but I think It is for the 16bit-data bus access control only. Not for the Memory array control of the SRAM,  right ?

T J
Senior III
Feb 27, 2017 8:24 AM UTC
Posted on February 27, 2017 at 08:24

<edited after understanding>

Usually you do connect the /UB and /LB pins, yes.

I checked the cubeMX file. attached

the 100pin processor does not give you the functionality.

I went to the 144 pin.

2^ 19 =512k (A0-A18 is 19 pins)

2^ 20 = 1M (A0-A18 with UB and LB strobes)

The pins /UB and /LB are used like another A0 physically.

Wire /UB, /LB and A0-A18, from the MCU to the SRAM, then you will have the necessary 20 address pins.

see link below:-

.

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2F27%2Fbf%2Ff5%2Fe8%2Fd7%2F82%2F44%2F6f%2FCD002004pdf%2Ffiles%2FCD002004pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.CD002004pdf

Thanks to

https://community.st.com/people/Kaltofen.Jupp?et=watches.email.thread

for the excellent work.

________________

Attachments :

F417ZGT 144 pin SRAM.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyry&d=%2Fa%2F0X0000000bDN%2FV7C74hNp8tV5cPIeDYjZygTL9E1cI3fJMxx0TQohQo8&asPdf=false
world04
Visitor II
Feb 27, 2017 9:17 PM UTC
Posted on February 27, 2017 at 21:17

Ok, your example has a wrong address range declaration - not 20Bit, just 19Bit. Connect the lines UB# and UL# to NBL0 and NBL1.The sram address lines A0 to A18 should connect with A0 to A18 of the MPU. The 'ByteEnable' lines are used by this SRAM config and map's NBL0 and NBL1 to the control bus. To use them as an A0 line to flip the low- and high-byte's will not work.

I had not further checked your system timing that the MXCube generate, but i have cleanup the code to get a more overview and comment some lines of code to mak up them for what this stay's for and the purpose of them.

http://www.st.com/content/ccc/resource/technical/document/application_note/27/bf/f5/e8/d7/82/44/6f/CD002004pdf/files/CD002004pdf/jcr:content/translations/en.CD002004pdf

.The example link points to a document from st where the wiring is done and the schematic is useful.

I had used the HAL-lib and not the stdLib, that's often used up to F4 familiy controllers. This is more detailed and better fixed and upward compatible if you may use an newer controller's like the F7, where StdLib's are not available.

I will hope this will help's you to solve the problem finaly. If you had done this issue, lease release a detailed notice how you have done this. I had spend near one hour to recherche this replay - it would be nice for all other here, to find a complete thread.

Just a sentence to HAL and STDLIB for others:

I know there are always programmers out there who say, that you should neither use the one nor the other and instead of the better the register directly served - best in Assembler. Well, it is forgiven me, but I am not interested in any further discussion on the usefulness of this Libs. If you do not want to use it, you just have to leave it - no one is tamed to do so.

________________

Attachments :

TEST.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyoH&d=%2Fa%2F0X0000000bDM%2Fc2t_fKIsuyvqVt3MGHmiAP6y_6HR94Foidg1KLjhgq4&asPdf=false
world04
Visitor II
Feb 28, 2017 8:00 AM UTC
Posted on February 28, 2017 at 09:00

I assume the issue is solved now. The datasheet i pointed to, explain how the signaling must be done. It's not explain how the MPU handle the byte control pins. I am sure that this are not just placed into the A0 line.

If i have a board that requires external sram, i will check up how the f4 handles this lines.