Interfacing STM32 MCU to micro-LED (µLED) display.
Hi Community,
I am working on Interfacing STM32 MCU to VGA LED display through SPI protocol.
Display Power Requirement.
1) Core Supply Provided : 1.2V, 1000mA. (required 200mA)
2) IO Supply : 2.5V, 1000mA. (required 200mA)
3) Cathode Supply : -2V, 200mA. (required 100mA)
The VGA LED display is consuming right amount of power but not turning on. What may be the reason?
By using company's provided hardware, Software-tool (GUI) I am able to turn-ON the display, getting the device id and do the operations. But using our customized hardware and company's provided drivers neither device is turned ON nor getting the device id.
Awaiting for suggestions and support.
Regards,
Vins.