Skip to main content
cabecas
Associate
December 16, 2008
Question

interfacing sd/mmc card

  • December 16, 2008
  • 3 replies
  • 1004 views
Posted on December 16, 2008 at 03:19

interfacing sd/mmc card

    This topic has been closed for replies.

    3 replies

    janek
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:56

    Quote:

    On 15-12-2008 at 20:26, Anonymous wrote:

    Hi, can I interface a sd/mmc card with a STM32F103 without being with SPI interface?I want to capture video from a camera (VS6724) VGA 30 fps (only 20 seconds) and store in a memory card, I my question is if I can do that directly without buffer the video in a RAM.

    thank you

    Can I ask you, where did you get the camera from (VS6724)?

    I need a couple of them plus connectors for my project as well.

    If anyone knows a source of above please let me know.

    I had once the samples promised through an Australian distributor, but after a year of waiting the people from ST changed their minds and deny any samples even I was happy to pay for them.

    Jan

    relaxe
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:56

    You are limited to the SPI interface for all MCU without the SDIO interface. The STM32F103ZE on the STM3210E-EVAL have such a port.

    If your board/mcu supports it, there is an example application at exemples/sdio/sdcard with a multiblock-write sequence.

    Your limiting factor here is clearly speed, as you need to write a lot of data in a short timeframe. I suggest you run the example app with a very fast SDHC card (class 6), and benchmark your top speed. If it is not enough, nothing will do and you will need a ram buffer.

    On another thread called ''SDIO + Fat16/Fat32'' there is an exemple of a FAT32 application over SDIO and SPI so you can use normal windows compatible file system on your card.

    cabecas
    cabecasAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:56

    Hi, can I interface a sd/mmc card with a STM32F103 without being with SPI interface?I want to capture video from a camera (VS6724) VGA 30 fps (only 20 seconds) and store in a memory card, I my question is if I can do that directly without buffer the video in a RAM.

    thank you