Skip to main content
Visitor II
October 23, 2024
Question

Interfacing of Wave share 10.1DP-CAPLCD (capacitive touch) with STM32 series.

For my current project, I am seeking recommendations for the most suitable STM32 microcontroller series. Below are the specific requirements for my product:

  • Support for the Wave share 10.1-inch DP-CAPLCD with HDMI connectivity, along with integrated touch functionality.
  • At least 40 General Purpose Input/Output (GPIO) pins.
  • A minimum of 3 UART interfaces.
  • 4 to 5 I2C interfaces.
  • Support for timers.

For Now I am wiling to use STM32H7S7A8 module to interfacing Display using HDMI and for touch.

Do I need to add external hardware for display or it will directly work with this STM series. And for touch also verify does it require any external hardware for touch also??

If it requires some interface please specify that one.

This topic has been closed for replies.