Skip to main content
PJose.1
Associate
March 4, 2021
Question

Interface CAN with STM32f4 and STM32f091

  • March 4, 2021
  • 3 replies
  • 1079 views

HI

I am trying to interface Stm32f407board with cjmcu2551 transceiver with tcan1051V module and stm32f091cct6.the clock rate for both controllers(APB1 for CAN=25Mhz) with prescalar=5, time segment1=8 and time segment 2=1 with baud rate 500kbps. i am not able to get CAN communcaition between two. but when 2 stm32f407and mcp2551 transceiver with the same configuration is workling fine. I am using 2 functions HAL_CAN_RxFifo0MsgPendingCallback and HAL_CAN_TxMailbox0CompleteCallback for transmission and reception. i feel that nothing happening on stm32f091 can side. please suggest solutions. thanks

This topic has been closed for replies.

3 replies

Ozone
Principal
March 4, 2021

Some formatting would make the post more readable.

Having a proper termination resistor added ?

Are there signals visible on the bus ?

Are the connections (CanH,CanL) correct ? Have you tried to swap ?

Does the error counter on the sending node go up ?

PJose.1
PJose.1Author
Associate
March 4, 2021

Sorry for the formatting

Yes there are 120ohm termination on both ends

No signals are visible on the bus

Yes CANH and CANL are connected with 2 modules(not interchanged)

how can I check the error counter ?

Ozone
Principal
March 4, 2021

CAN peripherals require a transmit and a receive error counter, according to the standard.

They are usually available in the CAN peripheral status registers.

I didn't work with STM32 CAN lately, only MCUs from other vendors.

After a certain amount of successive fails, a node goes from error_active into error_passive mode, or bus_off mode.

Are the static levels correct if both boards are connected ?

Have you tried to connect them directly, i.e. bypassing the transceivers ?

Only watch out for proper power supply, best option is to supply both boards from the same supply in this case.