Skip to main content
Tkamaal
Associate II
Jan 10, 2018 2:39 AM UTC
Question

Integrate X-CUBE-MEMSMIC1 package with STM32L4 MCU

Posted on January 10, 2018 at 03:39

Hello,

I have couple of questions, 

1. I would like to know, if I can use X-CUBE-MEMSMIC1 package with Digital MEMS Mic that I have instead of using X-NUCLEO-CCA02M1 MEMS Evaluation board. If so, how can I do it? 

2. Can I modify the X-CUBE-MEMSMIC1 package projects (particularly AcousticBF) to work on STM32L471. 

According to documentation, I should be able to modify the project source code to run on STM32L471. But I would like to if anyone else has tried doing soomething similar. 

Regards. 

    This topic has been closed for replies.

    1 reply

    Bogdan Golab
    Lead
    Jan 10, 2018 6:57 AM UTC
    Posted on January 10, 2018 at 07:57

    Topic touched several times on this forum - I mean different boards but problem is the same.The CubeMX does not allow to automatically integrate BSP packages (drivers for nucleo modules, or other stuff on the discovery boards) with cube generated projects. So you have to manually modify delivered examples (needs some experience) OR generate the project automatically using CubeMX for resources required by particular board.

    See my posts:

    https://community.st.com/0D50X00009bMM7ESAW

    https://community.st.com/0D50X00009XkYoaSAF