Skip to main content
nanayakkaraan
Associate III
October 29, 2010
Question

Inserting asm instructions in C

  • October 29, 2010
  • 4 replies
  • 3364 views
Posted on October 29, 2010 at 14:10

Inserting asm instructions in C

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:13

    Try:
     __asm 
    volatile
    (
    ''cpsie i''
    );

    __asm
    (
    ''cpsie i''
    );
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:13

    In the specific case of CPSIE, search your compiler manuals for something similar to this:

    http://www.keil.com/support/man/docs/armcc/armcc_CHDFGFAB.htm#Ciabijcc

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:13

    ''I need (sic?) to insert some assembly code into my C code''

    Do you - really?!

    In many (most?) cases, this approach is fundamentally flawed:

    When you write in a High-Level Language (HLL) such as 'C', you delegate responsibility for code generation and the management of CPU resgisters, etc, to the Compiler - if you just ''jump in'' with the odd piece of arbitrary assembler code you are highly likely to mess stuff up!

    So, what is it that you feel cannot be done in 'C', and yet will be safe to just insert arbitrarily into the middle of a 'C' file?

    You will need a thorough understanding of what is and is not safe to fiddle with and what can and cannot be relied upon for your particular version of your particular compiler.

    If you have something that really does need to be in assembler, it's usually better to put it into a proper assembler routine in a proper assembler source file of its own and call that from 'C.

    Well, that's my 2p...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:13

    See: 

    http://www.keil.com/forum/17856/

    Here's a good paper from ARM TechCon about mixing assembler with High-Level Languages (HLLs) such as C and C++

    http://www.eetimes.com/design/embedded/4210485/Reliable-programming-in-ARM-assembly-language?pageNumber=0

    Note particularly the comment about inline assembly:

    ''While [inline assembly] may be an acceptable mechanism for somebody familiar with the inner workings of the ... compiler to provide assembly capabilities, they are very dangerous in the hands of a novice.''

    It seems to me that the vast majority of questions about inline assembler on this (and other) forums are from novices - and, thus, are generally bad ideas.

    The article outlines 3 ways to access assembler functionality, in order of preference:

    1. First, use Compiler Intrinsics wherever possible;

    2. Use separate assembler source files, with functions to be called from the HLL;

    3. As a last resort, and only for experienced developers, use inline assembler.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.