Skip to main content
HungKai.Chien
Associate II
Jul 31, 2025 1:49 AM UTC
Solved

Inquiry on STM32G0 Support for Dual USB-C Ports with DRP and DP-Alt Mode

I am currently evaluating the STM32G0 series for a project that requires two USB Type-C ports.
Each port needs to support both Dual Role Port (DRP) functionality and DisplayPort Alternate Mode (DP-Alt).
Can the STM32G0 be implemented?

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
Aug 4, 2025 1:54 PM UTC

Hi @HungKai.Chien 

Indeed, it is the same controller available on both ports. So, they have the same features.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

3 replies

ST Technical Moderator
Aug 1, 2025 10:32 AM UTC

Hi @HungKai.Chien 

Indeed, STM32G0 is the only product using 2 USB type C ports.

You can refer to the MB1352 schematics of STM32G0C1 eval daughter board as a reference.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
HungKai.Chien
Associate II
Aug 4, 2025 12:55 AM UTC

Hi Support team,


Does each UCPD port on STM32G0C1 support both DRP and DP-Alt mode independently?”

FBLBest answer
ST Technical Moderator
Aug 4, 2025 1:54 PM UTC

Hi @HungKai.Chien 

Indeed, it is the same controller available on both ports. So, they have the same features.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL