Skip to main content
Visitor II
March 3, 2025
Question

Inquiry on selecting MCU's for wireless transmission

Hi there,

We are working on a project in university. The objective of the project is to wirelessly transmit live camera feed to a LCD MIPI-4 Lane 50 pin screen using a digital camera module. We plan on using two microcontrollers, one for the camera which is remotely placed and one for the LCD screen that is with the user. We are wondering whether the STM32 boards we are looking to acquire are applicable for our intended applications or if any adjustments should be made. 
Choice for camera microcontroller:

  • Looking at STM32N6 series

Choice for display microcontroller:

  • STM327B3I-DK
  • STM32H747

We are also unsure how to wirelessly transmit the feed (up to 2 miles), please suggest solutions for STM32 Microcontrollers as well.

 

Thank you,
Chris

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
March 4, 2025

Perhaps you should look at what resolutions and protocols UAV video solutions are using and the kinds of bandwidth and power involved

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..