Skip to main content
Associate II
June 14, 2024
Question

Initialize the bootloader on STM32L432KC

I am a new embedded software engineer using STM32L432KC for my company's projects.

I have been tasked to install a bootloader into this MCU. I am not sure how to proceed. I do understand that the BOOT0 pin which is grounded has to be set HIGH and BOOT1 pin has to be set LOW. But I'm not sure how to program the chip to install the bootloader into memory.

Can someone assist me on this issue? I am using the Keil Microvision alongside STM32CubeMX. 
It would be really helpful if you could prove the links to APIs/Headerfiles etc/.

This topic has been closed for replies.

5 replies

STTwo-32
ST Technical Moderator
June 14, 2024

Hello @Abijith and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you follow the instructions and recommendations of the AN2606. Also, you have to take a look at the chapter 2.6 of the RM0394.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AbijithAuthor
Associate II
June 19, 2024

Hey, thanks for the reply.

Is it possible to flash the firmware using GPIO pins via UART? I would not want to use microUSB anymore. This is because my company is building a tool with other components and it will be difficult to open the packaging every time to connect the microUSB and flash.

 

MM..1
Super User
June 19, 2024

Your inf is little chaos, from where you have here micro USB? But primary you can use own bootloader = any custom method and connection for fw, or sytem bootloaders as described in AN2606 actualy chapter 66 pages 329-...

ST Employee
June 17, 2024

Hi All,

 

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

 

Regards,

Jake

ST Support