Skip to main content
claire
Associate II
May 14, 2012
Question

incrementation of a timer : problem

  • May 14, 2012
  • 11 replies
  • 2900 views
Posted on May 14, 2012 at 17:40

hi,

i am working on the stm32discovery

i am trying to increment a timer (timer2 channel 1) each time the signal on the pin PA.05 is rising but the timer is random incrementing and not at each rising edge of the signal

i don't understand why ?

here is my code :

int main(void)

{

    /* Configure Clocks for Application need */

    RCC_Configuration();

    /* Configure RTC Clocks */

    //RTC_Configuration();

      /* Configure SysTick IRQ and SysTick Timer to generate interrupts every 500µs */

    RCC_GetClocksFreq(&RCC_Clocks);

    //SysTick_Config(RCC_Clocks.HCLK_Frequency / 2000);

    /* Enable GPIOs clock */     

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE);

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,ENABLE);

    /*PA.05 TIM2 channel 1*/

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;

    GPIO_Init(GPIOA,&GPIO_InitStructure);

    GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_TIM2);

    TIM_InitStruct.TIM_Period = 849;

    TIM_InitStruct.TIM_Prescaler = 0;

    TIM_InitStruct.TIM_CounterMode = TIM_CounterMode_Up;

    TIM_TimeBaseInit(TIM2,&TIM_InitStruct);

    /*timer2 chanel 1  ETR pin PA5*/

    TIM_ICInitStruct.TIM_Channel = TIM_Channel_1;

    TIM_ICInitStruct.TIM_ICPolarity = TIM_ICPolarity_Rising;

    TIM_ICInitStruct.TIM_ICSelection  = TIM_ICSelection_DirectTI;

    TIM_ICInitStruct.TIM_ICPrescaler = TIM_ICPSC_DIV1;

    TIM_ICInitStruct.TIM_ICFilter = 0x0;

    TIM_ICInit(TIM2, &TIM_ICInitStruct);

    /*enable the TIM counter*/

    TIM_Cmd(TIM2, ENABLE);

    TIM_TIxExternalClockConfig(TIM2, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0);

    TIM_ETRClockMode1Config(TIM2,TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted,0);

  while (1){

      SysTick_Config(RCC_Clocks.HCLK_Frequency / 2000);

    bitStatut = GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_5);

    increment = TIM_GetCapture1(TIM2);

    Delay(100);

  }

could you help me ?

thanks
    This topic has been closed for replies.

    11 replies

    Tesla DeLorean
    Guru
    May 14, 2012
    Posted on May 14, 2012 at 19:36

    I'd start by taking the SysTick_Config(RCC_Clocks.HCLK_Frequency / 2000); out of the loop, what's that supposed to do?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    claire
    claireAuthor
    Associate II
    May 14, 2012
    Posted on May 14, 2012 at 19:46

    unfortunatelly that doesn't change a thing the timer is still incrementing random and not only on the rising edge maybe it is a initialisation missing ?

    Tesla DeLorean
    Guru
    May 14, 2012
    Posted on May 14, 2012 at 21:30

    But what was the purpose of having that within the loop, I'm trying to understand why.

    What is the nature of the input signal, please describe the frequency/period and duty cycle?

    If you are pushing a button, you might see contact bounce.

    Do you have any interrupt code servicing the SysTick?

    How long is Delay(100) ?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    May 14, 2012
    Posted on May 14, 2012 at 23:54

    Here's how I'd demonstrate this on an STM32 VL-Discovery with the Keil Evaluation, and serial cable attached to USART1. I don't have an STM32 L-Discovery board to hand, YMMV.

    Counts clocks on TIM1_ETR from a clock source running at 1 Hz, in this case generated on TIM4_CH1 and looped back externally. It counts off seconds, wrapping at 3600 (1 Hour), shows also the delta between the last counter measurement if the printf eats too many cycles.

    // sourcer32@gmail.com - STM32 VLDiscovery 1HZ External clock demo
    #include <
    stdio.h
    >
    #include ''stm32F10x.h''
    #include ''STM32vldiscovery.h''
    /**************************************************************************************/
    void RCC_Configuration(void);
    void GPIO_Configuration(void);
    void TIM4_Configuration(void);
    void TIM2_Configuration(void);
    void USART_Configuration(void);
    /**************************************************************************************/
    int main(void)
    {
    uint16_t LastTick, CurrentTick;
    RCC_Configuration();
    USART_Configuration(); // For DEBUG
    GPIO_Configuration();
    TIM4_Configuration(); // 1Hz Output
    TIM2_Configuration(); // Count input clock
    // Pin PB.06 (TIM4_CH1) looped back to PA.00 (TIM2_ETR) externally
    // Print a tick everytime the counter changes
    LastTick = TIM_GetCounter(TIM2) - 1;
    while(1)
    {
    CurrentTick = TIM_GetCounter(TIM2);
    if (CurrentTick != LastTick)
    {
    printf(''Tick:%5u Delta:%5u
    '', CurrentTick, (uint16_t)(CurrentTick - LastTick));
    LastTick = CurrentTick;
    }
    }
    }
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    // clock for GPIO
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB, ENABLE);
    // clock for TIM2 & TIM4
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM4, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    // PB.06 TIM4_CH1
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_Init(GPIOB, &GPIO_InitStructure);
    // PA.00 TIM2_ETR
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    }
    /**************************************************************************************/
    void TIM4_Configuration(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure;
    // Set up TIM4_CH1 to be a 1 Hz time base (1PPS)
    TIM_TimeBaseStructure.TIM_Prescaler = 24000 - 1; // 24 MHz / 24000 = 1 KHz
    TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // 1 KHz / 1000 = 1 Hz
    TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
    // Channel 1 configuration = PB.06 TIM4_CH1
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = (TIM_TimeBaseStructure.TIM_Period + 1) / 2; // 50% Duty
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OC1Init(TIM4, &TIM_OCInitStructure);
    // turning on TIM4 and PWM outputs
    TIM_Cmd(TIM4, ENABLE);
    TIM_CtrlPWMOutputs(TIM4, ENABLE);
    }
    /**************************************************************************************/
    void TIM2_Configuration(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_TimeBaseStructure.TIM_Prescaler = 0;
    TIM_TimeBaseStructure.TIM_Period = 3600 - 1; // 1 Hour in seconds
    TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
    // PA.00 TIM2_ETR
    TIM_ETRClockMode1Config(TIM2, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0);
    // TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_External1);
    TIM_Cmd(TIM2, ENABLE);
    }
    /**************************************************************************************/
    void USART_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    USART_InitTypeDef USART_InitStructure;
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
    /* Configure USART Tx as alternate function push-pull */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; // PA.09 USART1.TX
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* Configure USART Rx as input floating */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; // PA.10 USART1.RX
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    /* USART resources configuration (Clock, GPIO pins and USART registers) ----*/
    /* USART configured as follow:
    - BaudRate = 115200 baud
    - Word Length = 8 Bits
    - One Stop Bit
    - No parity
    - Hardware flow control disabled (RTS and CTS signals)
    - Receive and transmit enabled
    */
    USART_InitStructure.USART_BaudRate = 115200;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    /* Enable UART clock */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
    /* USART configuration */
    USART_Init(USART1, &USART_InitStructure);
    /* Enable the USART1 */
    USART_Cmd(USART1, ENABLE);
    }
    /**************************************************************************************/
    #include <
    rt_misc.h
    >
    #pragma import(__use_no_semihosting_swi)
    struct __FILE { int handle; /* Add whatever you need here */ };
    FILE __stdout;
    FILE __stdin;
    int sendchar(char c)
    {
    while((USART1->SR & 0x80)==0); // 80 = TXE, 40 = TC
    USART1->DR = c;
    return(1);
    }
    int getkey(void)
    {
    while((USART1->SR & 0x20)==0); // 20 = RXNE
    return(USART1->DR);
    }
    int fputc(int ch, FILE *f)
    {
    if ((char)ch == '
    ')
    sendchar('
    ');
    return (sendchar((char)ch));
    }
    int fgetc(FILE *f) {
    return (getkey());
    }
    int ferror(FILE *f) {
    /* Your implementation of ferror */
    return EOF;
    }
    void _ttywrch(int ch)
    {
    if ((char)ch == '
    ')
    sendchar('
    ');
    sendchar((char)ch);
    }
    void _sys_exit(int return_code) {
    label: goto label; /* endless loop */
    }
    /**************************************************************************************/
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {
    }
    }
    #endif
    /**************************************************************************************/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    claire
    claireAuthor
    Associate II
    May 15, 2012
    Posted on May 15, 2012 at 08:29

    i am sending a square wave on the pin PA.05 and i simply want to increment it of 1 at each rising edge starting from 0

    i put the delay of 100ms because the clock int the loop was too fast to be abble to detect my square wave

    claire
    claireAuthor
    Associate II
    May 15, 2012
    Posted on May 15, 2012 at 08:30

    the signal is a simply square wave of frequency 100Hz and a duty cycle of 50%

    claire
    claireAuthor
    Associate II
    May 15, 2012
    Posted on May 15, 2012 at 10:36

    it is working in low frequency

    thanks for the help

    carl239955_st
    Visitor II
    February 25, 2013
    Posted on February 25, 2013 at 12:45

    I have almost the same problem:

    I have a flowmeter that makes pulses that I want to count. The frequency is variable between 0 and 20kHz. During design I can control the flow. The board is a keil MBCSTM32 Board. To test the example on this thread I have connected my flow-signal both to ETR (PD2) and to TI1 (remaped to PC6).

    When I try to read the input bitwise through the GPIO i get the signal but doing the same through the timer, TIM3_GetValue(TIM3) returns 0. I have the feeling it is easy to solve but I am truly stuck.

    #include ''lcd.h''

    #include ''stm32f10x_tim.h''

    #include ''stm32f10x_gpio.h''

    void hw_init();

    int main(void)

    {

        hw_init();

        long count = 1;

        unsigned char last_bit = 0;

        long l_sum = 0;

        uint32_t l;

        while(1)

        {

    /*

    //        l=GPIO_ReadInputDataBit(GPIOC,GPIO_Pin_6); // Testing pin input

            l=GPIO_ReadInputDataBit(GPIOD,GPIO_Pin_2); //

            if(l!=last_bit && l==1)

            {

                l_sum++;

            }

            last_bit = l;

    */

            if(!count --)

            {

                count = 1000000;

                l=TIM_GetCounter(TIM3);

                lcd_set_position(1,5);

    //            lcd_write_int(l_sum); // Works

                lcd_write_int(l);

            }

        }

    }

    void hw_init()

    {

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD ,ENABLE);

        RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

        lcd_init(LCD_4_BIT_BUS,LCD_FONT_5x11); // Uses PC0-4 and PC10-12

        // --- Timer3 ---

        // PC6 & PD2 are both connected to the same input signal from flowmeter

        GPIO_StructInit(&gpio_struct);

        gpio_struct.GPIO_Pin = GPIO_Pin_6 ;

        gpio_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING;

        GPIO_Init( GPIOC, &gpio_struct);

        GPIO_StructInit(&gpio_struct);

        gpio_struct.GPIO_Pin = GPIO_Pin_2 ;

        gpio_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING;

        GPIO_Init( GPIOD, &gpio_struct);

        TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct;

        TIM_TimeBaseStructInit(&TIM_TimeBaseInitStruct);

        TIM_TimeBaseInitStruct.TIM_CounterMode = TIM_CounterMode_Up;

        TIM_TimeBaseInit(TIM3, &TIM_TimeBaseInitStruct);

    #ifdef USE_TRIGGER_INPUT_1

        GPIO_PinRemapConfig(GPIO_FullRemap_TIM3,ENABLE);

        TIM_ETRClockMode2Config(TIM3,TIM_ExtTRGPSC_OFF,TIM_ExtTRGPolarity_NonInverted,0);

        TIM_ICInitTypeDef TIM_ICInitStruct;

        TIM_ICStructInit(&TIM_ICInitStruct);

        TIM_ICInit(TIM3,&TIM_ICInitStruct);

        TIM_TIxExternalClockConfig(TIM3,  TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0);

        TIM_CCxCmd(TIM3,TIM_Channel_1,TIM_CCx_Enable);

    #else // USE_TRIGGER_INPUT_1

        TIM_ETRClockMode1Config(TIM3,TIM_ExtTRGPSC_OFF,TIM_ExtTRGPolarity_NonInverted,0);

    #endif

    //    TIM_ETRClockMode1Config(TIM3,TIM_ExtTRGPSC_OFF,TIM_ExtTRGPolarity_NonInverted,0);

    //    TIM_SelectSlaveMode(TIM3, TIM_SlaveMode_External1);

        TIM_Cmd(TIM3, ENABLE);

    }

    Tesla DeLorean
    Guru
    February 25, 2013
    Posted on February 25, 2013 at 18:13

    Counting button (B1) presses on the VL-Discovery, uses TIM2 CH1 PA0

    void TIM2_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; // PA2 TIM2_CH1 BUTTON 1
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    TIM_TimeBaseStructure.TIM_Period = 65535;
    TIM_TimeBaseStructure.TIM_Prescaler = 0;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
    TIM_TIxExternalClockConfig(TIM2, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0);
    TIM_Cmd(TIM2, ENABLE);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    February 25, 2013
    Posted on February 25, 2013 at 18:21

    Bonding PC6 to PA0 button input

    void TIM3_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE); // AFIO required for remapping
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; // PC6 TIM3_CH1
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE);
    TIM_TimeBaseStructure.TIM_Period = 65535;
    TIM_TimeBaseStructure.TIM_Prescaler = 0;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
    TIM_TIxExternalClockConfig(TIM3, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0);
    TIM_Cmd(TIM3, ENABLE);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..