Skip to main content
Muhammet TAN
Associate II
April 4, 2018
Question

Increase the intensity of white led

  • April 4, 2018
  • 3 replies
  • 2111 views
Posted on April 04, 2018 at 17:29

Hi , I want to drive White Led 7 Segment Display. MCUs power supply is 3.3V (STM32F030C6T6), and white led voltage about 2.8V when the current is 20mA. So, light intensity is too low. Is there any way to increase intensity or need to use STM8S005C6T6 ? 

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    April 4, 2018
    Posted on April 04, 2018 at 19:29

    Could you use a buffer capable of delivering more current?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Muhammet TAN
    Associate II
    April 4, 2018
    Posted on April 04, 2018 at 20:27

    I have only a ULN2003APW but 7 segment display is common cathode. the company do not use buffer like 74hc series or cd4511. 

    T J
    Senior III
    April 4, 2018
    Posted on April 05, 2018 at 00:42

    You can use a transistor, good for upto 1 Amp.

    or a FET good for 80A.

    Muhammet TAN
    Associate II
    April 5, 2018
    Posted on April 05, 2018 at 07:26

    Actually we've thought this. So there are so many component on the board. because there are three 7-segment displays. maybe using stm8 is more useful than stm32 for this circuit. 

    T J
    Senior III
    April 5, 2018
    Posted on April 05, 2018 at 07:42

    MM5450  in the old days,

    or

    https://www.digikey.com.au/product-detail/en/sparkfun-electronics/COM-11442/1568-1346-ND/5824095

     

    currently.