Incorrect STM32F4 svd files?
So I downloaded en.stm32f4_svd which contains the System View Description (SVD) files for the complete range of F4's
Looking at the STM32F429.svd in particular even though I believe they are all incorrect we have the following...
Under the CPU section there seem to be some values at odds with ST's data sheets, and header files
revision is set as r1p0 rather than r0p1
mpuPresent and fpuPresent are set as false when clearly they are present
nvicPrioBits is set to 3 when in should be 4
Am I misunderstanding something or are these values actually wrong or have I downloaded outdated files (v1.2) ?
Here's the link to the download