Skip to main content
Associate II
August 6, 2024
Solved

Inconsistency Error during In-Application Firmware Update on STM32H7

 

Hello everyone,

I'm working on an in-application firmware update for an STM32H7 series microcontroller. The process involves erasing and then writing to the flash memory. I can successfully erase bank 2, but I'm encountering an issue when writing to the flash.

Issue Description: After the first 256 bits (flash-word) are written without any error, the subsequent write operations result in an inconsistency error. Interestingly, even though the HAL_FLASH_Program function returns an error, when I compare the write buffer with the flash memory, all the data appears to have been written correctly.

Code Snippet:

HAL_StatusTypeDef flash_write(uint32_t address, uint8_t* data, size_t size) {
 HAL_StatusTypeDef status = HAL_OK;

 HAL_FLASH_Unlock();
 for (size_t i = 0; i < size; i += 8) {
 if (address + i <= (FLASH_END_ADDRESS - 8)) {
 status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, address + i, (uint32_t )data + i);
// if (status != HAL_OK) {
// break; // Exit if there's an error
// }
 // Verify the content of flash with RAM
 if (*(uint32_t*)(address + i) != *(uint32_t*)(data + i)) {
 status = HAL_ERROR; // Set an error status if verification fails
 break;
 }
 else {
 	status = HAL_OK;
 }
 } else {
 status = HAL_ERROR; // Set an error status if out of bounds
 break;
 }
 }
 HAL_FLASH_Lock();

 return status; 
}

Observations:

  1. The first write operation succeeds, but subsequent ones return an error despite the data being written correctly.
  2. I've included a verification step after writing each 256-bit flash-word, which confirms that the data in flash matches the data in the RAM.

Questions:

  • Has anyone encountered a similar issue with the STM32H7 series or other STM32 series?
  • Could this be a known issue with the HAL library or something related to the specific flash memory behavior?
  • Are there any recommended steps or checks to perform when encountering such inconsistencies?

Any insights or suggestions would be greatly appreciated!

This topic has been closed for replies.
Associate II
August 6, 2024

I found the issue, and it turns out to be a simple mistake on my part. I mistakenly increased the iteration pointer by 8 instead of 8 * 4. That was causing the problem.

Based on the reference manual:

A wrap burst request issued by a master overlaps two or more 256-bit flash-word addresses, i.e. wrap bursts must be done within 256-bit flash-word address boundaries.

This misalignment was causing the inconsistency error I encountered. Correcting the iteration step resolved the issue.

Thank you all for your help and suggestions!

3 replies

TDK
August 6, 2024

This is almost certainly a caching issue.

Make the pointer which reads from flash volatile (volatile uint32_t*) which forces the cpu to read it every time.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
August 6, 2024

 

Thank you so much for your reply!

I appreciate your suggestion about making the pointer volatile. However, in my case, I'm passing a constant value as parameters like this:

 

 
if(flash_write(0x08100000, (uint8_t *)0x92000000, 205556) == HAL_OK)

Inside the HAL_FLASH_Program function, the addresses are already cast to volatile pointers:

 

 
__IO uint32_t *dest_addr = (__IO uint32_t *)FlashAddress;
__IO uint32_t *src_addr = (__IO uint32_t*)DataAddress;

This should inherently make the pointers volatile. Additionally, I've tried disabling the cache and using zero compiler optimization, but the issue still persists.

Could there be any other reasons for this inconsistency error, or perhaps something specific to the STM32H7 flash memory behavior?

saeed.poorjandaghiAuthorBest answer
Associate II
August 6, 2024

I found the issue, and it turns out to be a simple mistake on my part. I mistakenly increased the iteration pointer by 8 instead of 8 * 4. That was causing the problem.

Based on the reference manual:

A wrap burst request issued by a master overlaps two or more 256-bit flash-word addresses, i.e. wrap bursts must be done within 256-bit flash-word address boundaries.

This misalignment was causing the inconsistency error I encountered. Correcting the iteration step resolved the issue.

Thank you all for your help and suggestions!