Skip to main content
WFouq.1
Associate II
March 17, 2022
Solved

Im working on a project where I use the STM32L432 as slave while a Raspberry Pi is the master. The dataprotocol is I²c and im using the HAL_I2C library. But I cant transmit or receive data. Can someone help me with this?

  • March 17, 2022
  • 9 replies
  • 4488 views

I think i correctly setted up the slave adress on 0x70 with the configuration window.

Below my script on the Raspberry Pi.

0693W00000KczS2QAJ.png 

#include "main.h"
#include "string.h"
#include "stdio.h"
 
 
 
I2C_HandleTypeDef hi2c1;
 
UART_HandleTypeDef huart2;
 
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_I2C1_Init(void);
 
 
int main(void)
{
 
 
 HAL_Init();
 
 char msg[10];
 int buf[12];
 
 SystemClock_Config();
 
 
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_I2C1_Init();
 
 while (1)
 {
	 if( HAL_I2C_Slave_Receive(&hi2c1, (uint8_t*)msg, 2, HAL_MAX_DELAY) != HAL_OK){
		 strcpy((char*)buf, "Error Rx\r\n");
	 }else{
		 strcpy((char*)buf, "OK Rx\r\n");
	 }
 
 
 
		 HAL_UART_Transmit(&huart2, (uint8_t*)buf, strlen((char*)buf), HAL_MAX_DELAY);
		 HAL_Delay(500);
 }
 
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 16;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Enable MSI Auto calibration
 */
 HAL_RCCEx_EnableMSIPLLMode();
}
 
/**
 * @brief I2C1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_I2C1_Init(void)
{
 
 /* USER CODE BEGIN I2C1_Init 0 */
 
 /* USER CODE END I2C1_Init 0 */
 
 /* USER CODE BEGIN I2C1_Init 1 */
 
 /* USER CODE END I2C1_Init 1 */
 hi2c1.Instance = I2C1;
 hi2c1.Init.Timing = 0x00707CBB;
 hi2c1.Init.OwnAddress1 = 224;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Analogue filter
 */
 if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Digital filter
 */
 if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C1_Init 2 */
 
 /* USER CODE END I2C1_Init 2 */
 
}
 
/**
 * @brief USART2 Initialization Function
 * @param None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{
 
 /* USER CODE BEGIN USART2_Init 0 */
 
 /* USER CODE END USART2_Init 0 */
 
 /* USER CODE BEGIN USART2_Init 1 */
 
 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */
 
 /* USER CODE END USART2_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);
 
 /*Configure GPIO pin : LD3_Pin */
 GPIO_InitStruct.Pin = LD3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LD3_GPIO_Port, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 

This topic has been closed for replies.
Best answer by S.Ma

Try to reduce the bit rate to 10kbps and try. If it works it maybe a latency issue.

9 replies

TDK
March 17, 2022

> But I cant transmit or receive data.

Why not? What happens when you try? Are the boards connected correctly? Can you view the signals on the line to verify which device isn't doing its job?

"If you feel a post has answered your question, please click ""Accept as Solution""."
WFouq.1
WFouq.1Author
Associate II
March 17, 2022

I simply connected the GND, SDA and SCL with each other (Raspberry Pi & STM32) but I can't even find the STM-board on the Raspberry Pi. (The script that I execute is the script above in the question). And my output in the Cube IDE only says "Error Rx".0693W00000Kd2QJQAZ.png

TDK
March 17, 2022

> And my output in the Cube IDE only says "Error Rx".

Find out why. Look at the ErrorCode parameter for guidance. A logic analyzer would be helpful here to verify signals. I2C needs appropriate pullups on both lines.

"If you feel a post has answered your question, please click ""Accept as Solution""."
WFouq.1
WFouq.1Author
Associate II
March 18, 2022

I connected 2 1kohm resistors from my SCL and SDA to my 3.3V as pullup. I also changed my code to this. But I do something wrong that my statement is not equal to HAL_OK. How can I make it true so he triggers the else loop?

0693W00000Kd79mQAB.png

Tesla DeLorean
Guru
March 18, 2022

Don't the IT functions return immediately? How's that going to work?

Wouldn't you need some stateful implementation via the call-backs?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bob S
Super User
March 18, 2022

Did you ever find out why your original code was returning an error from your HAL_I2C_Slave_Receive() call as @TDK​ mentioned? You have the HAL source - step into it and see why it is returning an error (and WHAT error it returns). Go back to your original code and get that working. Then think about going to interrupt mode (which means you need to fill in HAL callback functions).

S.Ma
S.MaBest answer
Principal
March 19, 2022

Try to reduce the bit rate to 10kbps and try. If it works it maybe a latency issue.

WFouq.1
WFouq.1Author
Associate II
March 22, 2022

It works, I can detect my STM32 now on my Raspberry Pi by changing the frequency on my raspberry pi and stm32 to 10kHz!