Skip to main content
SG.11
Visitor II
December 21, 2022
Question

Im facing CAN transmit error,HAL_CAN_ERROR_TX_TERR0 (0x00001000U) /*!< TxMailbox 0 transmit failure due to transmit error */. Can anyone guide me how to resolve this or what is the reason for this error. Im using a NUCLEO-F767ZI board.

  • December 21, 2022
  • 2 replies
  • 1224 views

..

This topic has been closed for replies.

2 replies

ST Technical Moderator
December 26, 2022

Hello @SG.11​ and welcome to the Community :)

I advise you to refer to the CAN examples available within STM32CubF7 MCU package.

Have a look at this post, this may help you.

It would be better to provide more details about your project and configuration, this will help Community users to answer you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Karl Yamashita
Principal
December 26, 2022

Show us snippets of the code you wrote

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source