Illogical Prescaler Behavior
I wanted to see what would happen when I set the prescaler for an interrupt lower and lower.
My expectation was that the main loop would lose out on it's share of processing time, but I was surprised when the results of my test were mixed.
Essentially, I figured something along the lines of a prescaler of 84-30 would all be fine, other than the main loop increasingly taking longer to process. Then everything below 30 would take so long, it would appear to hang.
Instead of my expectation being reality, the illogical came to be, where prescalers from 84-72 would be good, then suddenly 69-67 "hangs". Then 66-47 is good, but again it switches back to bad at 46 and 45.
It gets this back and forth mix that I just don't understand the reasoning.
I just used the STM32F4-Discovery main.c template with minor adjustments:
BSP_LED_Init(LED3);
TIM_Handle7.Instance = TIM7;
TIM_Handle7.Init.Period = 1;
TIM_Handle7.Init.ClockDivision = 0;
TIM_Handle7.Init.CounterMode = TIM_COUNTERMODE_UP;
TIM_Handle7.Init.RepetitionCounter = 0;
TIM_Handle7.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
uint32_t tickVal, lastTickVal = 0;
uint32_t lastLedToggleTick = 0;
uint32_t result = 0;
float calc = 0;
/* Infinite loop */
while (1)
{
tickVal = HAL_GetTick();
if (lastTickVal != tickVal)
{
if ((lastLedToggleTick + 500) >= tickVal)
{
BSP_LED_Toggle(LED3);
lastLedToggleTick = tickVal;
}
for (uint32_t prescaler = 44; prescaler > 0; prescaler--)
{//bad:71,69-67,46-45,35-34,31-26
//good:84-72,66-47,44-36,33-32
TIM_Handle7.Init.Prescaler = prescaler - 1;
result = HAL_TIM_Base_Init(&TIM_Handle7);
timerCounter = 0;
result = HAL_TIM_Base_Start_IT(&TIM_Handle7);
for (uint32_t y = 906; y > 0; y--) //Just some math I'll be experimenting with, but irrelevant except only for the work load.
{
if ((907 % y) == 0)
{
result = HAL_TIM_Base_Stop_IT(&TIM_Handle7);
calc = ((1 / (float)((uint32_t) 84000000 / (uint32_t) prescaler)) * (uint32_t) timerCounter);
result = HAL_TIM_Base_DeInit(&TIM_Handle7);
break;
}
}
}
lastTickVal = tickVal;
}
}The IRQ Handler's only job was to increment the timerCounter.
Can someone explain the effect that I'm seeing?