Skip to main content
Visitor II
April 4, 2024
Solved

IKS4A1 and Unicleo-GUI Issue

Hi,

I have purchased a sensor expansion board (X-NUCLEO-IKS4A1) for my board (NUCLEO - F446ZE). However, when I wanted to display the data on Unicleo-GUI, the GUI cannot detect anything, not even my firmware. I looked through the datasheet for Unicleo-GUI and I did not see IKS4A1 being a supported model for the GUI. Could this be the issue?

 

In terms of setting up the board, I basically followed "Getting started with X-CUBE-MEMS1 with STM32CubeMX" document, specifically the steps under section 7.2 --"Use of MEMS Library with sample applications for X-NUCLEO-IKS01A3 or X-NUCLEO-IKS02A1 or X-NUCLEO-IKS4A1". Am I following the wrong step?

Best.

    This topic has been closed for replies.
    Imen.DBest answer
    ST Technical Moderator
    April 5, 2024

    Hello @WinstonZ,

    Check the serial settings to interface with Unicleo-GUI: baud rate 921600 bps; 8 data bits; No parity; 1 stop bit; no hard flow control (as mentioned in the UM1859 - page 5)

    • UM1859: Getting started with the X-CUBE-MEMS1 motion MEMS and environmental sensor software expansion for STM32Cube.
    • UM2128: Getting started with Unicleo-GUI for motion MEMS and environmental sensor software expansion
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

    1 reply

    Imen.DBest answer
    ST Technical Moderator
    April 5, 2024

    Hello @WinstonZ,

    Check the serial settings to interface with Unicleo-GUI: baud rate 921600 bps; 8 data bits; No parity; 1 stop bit; no hard flow control (as mentioned in the UM1859 - page 5)

    • UM1859: Getting started with the X-CUBE-MEMS1 motion MEMS and environmental sensor software expansion for STM32Cube.
    • UM2128: Getting started with Unicleo-GUI for motion MEMS and environmental sensor software expansion
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks