IEEE 802.1AS Transparent Clock not working on STM32MP257 ETHSW (TTTech DEIP): correctionField stays 0 on forwarded Sync/Follow_Up
Environment
- Board: ATK-DLMP257B (STM32MP257), ST official Yocto image (X-LINUX-TSNSWCH)
- Kernel 6.6.48
- deptp 2.5.2 (Flexibilis DE-gPTP Edge daemon)
- Driver:
edgx_pfm_lkm(TTTech EDGE Platform Host Interface Driver)
Goal
Configure the on-board switch as an IEEE 802.1AS Peer-to-Peer Transparent Clock, so that forwarded Sync/Follow_Up frames carry the residence time in their correctionField.
Configuration (factory default, unmodified)
<Interface name="sw0p2"><profile>gptp</profile><mode>tc</mode><delay>p2p</delay></Interface>
<Interface name="sw0p3"><profile>gptp</profile><mode>tc</mode><delay>p2p</delay></Interface>
<Basic><one_step_clock>0</one_step_clock></Basic>
deptp.service is active. deptp_tool --get-tc-port-dataset returns valid data (faulty false, peer-mean-path-delay ≈ 145 ns), while deptp_tool --get-port-dataset returns error rejected — confirming that deptp is actually running in TC mode.
Topology
GM (PC) — sw0p2 [board] sw0p3 — Slave (PC). Both endpoints run linuxptp 4.0 with network_transport L2, delay_mechanism P2P, transportSpecific 1, and -H (hardware timestamping). The measured P2P path delay is stable at 152 ns ± 1.
Observations
- Simultaneous captures on both sides of the board, matched by sequenceId: the same Sync/Follow_Up frames (seq 19246–19252) were captured at both ingress and egress, and the
correctionFieldis byte-for-byte identical — all zero (20 frames,00 00 00 00 00 00 00 00). - The board's CPU only ever sees Pdelay (249 frames each on sw0p2 and sw0p3, all PdelayReq/PdelayResp/PdelayRespFU). Forwarded Sync/Follow_Up never reach the CPU at all.
- The correction path itself is alive: after setting
<output_delay>1000</output_delay>, the board's own outgoing Pdelay_Req carriescorr=65536(1 ns) — but in the same capture, the forwarded Sync/Follow_Up still show 0. - The kernel repeatedly logs
EDGX-BR-CORE: edgx_com_ts_find_tx(): TX timestamp lost(~8/s, matching deptp's Pdelay_Req rate), with a correspondingptp_port_pdelay_measurement: Missing timestampson the deptp side.
Already tried — none of these change the result
<one_step_clock>1</one_step_clock>syncmode="1588"in/etc/modprobe.d/edgx_sw_core.conf(dmesg confirmsSynchronisation mode (syncmode): 1588after reboot; correctionField still 0)- One-step vs. two-step (flag
0x0000/0x0200) × transportSpecific0/1— all four combinations <profile>ptp</profile>: rejected — deptp exits with status 1;<mode>BC</mode>:libptp.so.0only exportsPTP_PORT_TYPE_OC/PTP_PORT_TYPE_TC, so there is no boundary clock support- Frames sent to
01:80:C2:00:00:0Eare not forwarded by the board (5 injected, 0 received at the far end) - Full
stringsscan of/boot/6.6.48/kernel/**/*.koforresidence|correctionField|transparent clock: zero matches. Inedgx_pfm_lkm.kothe only PTP-related strings aresyncmodeandtimestamp.
Questions
- Does the STM32MP2 ETHSW support an 802.1AS transparent clock (residence-time correction) on the forwarding path?
- If yes, what is the correct configuration? Is this feature implemented in the deptp 2.5.2 /
edgx_pfm_lkmshipped in X-LINUX-TSNSWCH? - If not, is it planned for a future release?