Skip to main content
Associate II
Apr 23, 2024 1:11 PM UTC
Question

IEC60335 SelfTestLib

In our legacy STM32f103 project a ST library named "Self Test Library" is used. It has version 1.0, dated 10/01/2007. That library is certified according to IEC60335. I found it in an archive named IEC60335.zip, but I have no idea if that's the original archive name. Source files are named "stm32f10x_STL*.h/.c.

Is the library still maintained? 

Can the original archive be downloaded somewhere?

Are newer versions available?

This topic has been closed for replies.