Id hardware in OTP STM32f207
Hi everyone!
I am using 1 piece of hardware that uses an STM32f207igh6 that has a registration number on it (serial). However, every time the STM32 f207 chip is damaged, it is necessary to replace the chip with a new one, so that the registration number matches the application in use. Previously, an expert helped me to do that, he said need to generate OTP for chip with old id number (serial) of broken chip, he asked me to use stlink stm32 utility of the program. start reading from address 0x1FFF7800 size 400 of the brand new chip and send him this data. Then he sent me a flash file using ST Link V2. Everything went smoothly. But now I can't contact him anymore. Can anyone here help me with this problem?
Thanks!