Skip to main content
Visitor II
December 19, 2023
Solved

IBIS model STM32H5

I'm using STM32H573IIK6TR and I download its IBIS simulation model from st.com [stm32h562_563_573_ufbga201.ibs]

There are a lot of pin model, but i cannot understand what is the correlaction between the datasheet and ibis model.

For example: 

I'm using pin H14 as SDCLK in high speed mode.

In IBIS model pins have the following models: low speed (io8_ft_spi_ls_3v3), medium speed (io8_ft_spi_ms_3v3), fast speed (io8_ft_spi_fs_3v3) and high speed (io8_ft_spi_hs_3v3). 

In datasheet there are 4 mode: low, medium, high and very high.

So, I think that "high mode" in datasheet correspond to "fast speed" in IBIS model, but results don't correspond at all.

 

This topic has been closed for replies.
ELABI.1
ELABI.1Best answer
ST Technical Moderator
December 21, 2023

Hello @Katherine ,

 Yes, you're right, "high mode" in datasheet correspond to "fast speed".

You can refer to AN4803 application note and precisely section 4.2 "Model selector" and you can find that the bit code naming is aligned with the IBIS model.

We are going to align the naming, what is important is the code of bits 00 01 10 11 to use the model, and we'll fix it in coming release.

Thank you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Eya.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

ELABI.1
ELABI.1Best answer
ST Technical Moderator
December 21, 2023

Hello @Katherine ,

 Yes, you're right, "high mode" in datasheet correspond to "fast speed".

You can refer to AN4803 application note and precisely section 4.2 "Model selector" and you can find that the bit code naming is aligned with the IBIS model.

We are going to align the naming, what is important is the code of bits 00 01 10 11 to use the model, and we'll fix it in coming release.

Thank you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Eya.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.