Skip to main content
milan
Associate II
October 11, 2010
Question

IAR + STM32VLDISCOVERY won't flash MCU

  • October 11, 2010
  • 2 replies
  • 853 views
Posted on October 11, 2010 at 12:53

Hi,

i have a problem with this evalution board. I opened the project in EWARM 5.50 and tried to Download & Debug the base project(with blinking diodes), but i get this error message

Failed to load flash loader ..../FlashSTM32F100xB.flash

The debugging session could not be started. Either the debugger initialisation failed or the output file ..../DISCOVER.out was corrupted.

in the debug log window is

Loaded macro file: C:\IAR Systems\Embedded Workbench 5.4_2\arm\config\flashloader\ST\FlashSTM32F10xxx.mac

Failed to load flash loader: C:\IAR Systems\Embedded Workbench 5.4_2\arm\config\flashloader\ST\FlashSTM32F100xB.out

Failed to load flash loader: C:\IAR Systems\Embedded Workbench 5.4_2\arm\config\flashloader\ST\FlashSTM32F100xB.flash

Debugging without downloading works.

Can somebody help me pls?

#ewarm #stm32vldiscovery
    This topic has been closed for replies.

    2 replies

    gdoura.marwa
    Visitor II
    October 12, 2010
    Posted on October 12, 2010 at 17:37

    Hi,

    This is a known bug in EWARM 5.50 with value line flashloader. It is fixed in EWARM5.50.5.

    I advise you, if possible, to upgrade your EWARM version to 5.50.5 (available on IAR web site: www.iar.com).

    Else , you can use the attached patch to fix this problem with your installed version. It contains a readme that explains hosw to use it.

    Hope this helps,

    regards,

    VLINE.

    milan
    milanAuthor
    Associate II
    October 12, 2010
    Posted on October 12, 2010 at 18:06

    Thank you! this solved my problem.