Skip to main content
bruce
Associate III
April 7, 2008
Question

IAR Kickstart Question, STM32

  • April 7, 2008
  • 3 replies
  • 604 views
Posted on April 07, 2008 at 17:43

IAR Kickstart Question, STM32

    This topic has been closed for replies.

    3 replies

    bruce
    bruceAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:28

    I'm not sure if this is the best forum for this, but I have questions on how to compile some of the example code in the IAR Embedded WorkBench.

    For example, there's a USART example, (example 7) I'd like to compile and then download to my IAR STM32-SK demo board using the Jlink.

    The instructions say:

    In order to make the program work, you must do the following :

    - Create a project and setup all your toolchain's start-up files

    - Compile the directory content files and required Library files :

    + stm32f10x_lib.c

    + stm32f10x_usart.c

    + stm32f10x_gpio.c

    + stm32f10x_rcc.c

    + stm32f10x_nvic.c

    + stm32f10x_flash.c

    - Link all compiled files and load your image into either RAM or Flash

    - Run the example

    Can someone give me a step-by-step as to how to set this up in the IAR GUI?

    Thanks

    bruce
    bruceAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:28

    Thanks for your help, I got it working.

    For others: the um0427 directory he refers to is the ST function library um0427.zip file on the ST web site.

    thanks again.

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:28

    Under um0427\STM32F10xFWLib\FWLib\project there is a pre-configured example for EWARM4.42A. Just copy the content of FWLib\examples\USART\Example7 folder except stm32f10x_conf.h file to \STM32F10xFWLib\FWLib\project and then rebuild your project.

    PS: The example is for the STM32-Eval board so you need to update it according to your board.