Skip to main content
bicmosit
Associate
October 18, 2010
Question

iar embedded workbench help me

  • October 18, 2010
  • 1 reply
  • 699 views
Posted on October 18, 2010 at 20:22

iar embedded workbench help me

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:11

    Hy all,I am new user of iar,

    do you recommend a good manual that explains well the c, for example the types uint8_t??

    thanks

    Doesn't IAR ship it with a manual, or two? Try enquiring with the local IAR sales office.

    uint8_t is a typedef that explicitly defines a ''8-bit unsigned integer'', because 'C' doesn't intrinsically have size guarantees for char, int, long, etc. People often use ''unsigned char'', but a byte isn't always 8-bit, although it's fairly safe these days. As for books, K&R was always the classic reference.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..