Skip to main content
harry anders
Associate III
May 23, 2018
Question

IAP failure on writing in STM32f429

  • May 23, 2018
  • 2 replies
  • 607 views
Posted on May 23, 2018 at 13:54

I am writing a bootloader application that resides in sectors_0 (0x08000000-0x08003FFF) and sector_1 (0x08004000-0x08007FFF) of stm32f429. When the bootloader application starts up it erases sector_2(0x08008000-0x0800BFFF) and sector_3(0x0800C000-0x0800FFFF) of the flash memory. Then loads the main code from an SDCARD and writes it to sector_2 and sector_3.

I can successfully erase sector_2 and sector_3 but when trying to write to them, I get HAL_ERROR.

This is the relevant code:

  /* Unlock the Flash to enable the flash control register access *************/

     

     volatile uint32_t main_addr = 0x08008000;

     FLASH_If_Init();

      FlashProtection = FLASH_If_GetWriteProtectionStatus();

      pEraseInit.TypeErase = TYPEERASE_SECTORS;

      pEraseInit.Sector = FLASH_SECTOR_2;

      pEraseInit.NbSectors = 2;

      pEraseInit.VoltageRange = VOLTAGE_RANGE_3;

      if (HAL_FLASHEx_Erase(&pEraseInit, &SectorError) != HAL_OK)

      {

         /* Error occurred while page erase */

         while (1);

      }

      if(FLASH_If_Write(main_addr, (uint32_t *)buffer, (fno.fsize)/4)!= FLASHIF_OK) //writes are 32 bit

        {

         //error    

         while(1);

        }

Functions being used have been defined in the CUBE project section: STM32Cube\Repository\STM32Cube_FW_F4_V1.21.0\Projects\STM32446E_EVAL :

/**

  * @brief  Unlocks Flash for write access

  * @param  None

  * @retval None

  */

void FLASH_If_Init(void)

{

  HAL_FLASH_Unlock();

  /* Clear pending flags (if any) */  

  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR |

                         FLASH_FLAG_PGAERR | FLASH_FLAG_PGPERR | FLASH_FLAG_PGSERR);

}

/**

  * @brief  This function writes a data buffer in flash (data are 32-bit aligned).

  * @note   After writing data buffer, the flash content is checked.

  * @param  FlashAddress: start address for writing data buffer

  * @param  Data: pointer on data buffer

  * @param  DataLength: length of data buffer (unit is 32-bit word)   

  * @retval 0: Data successfully written to Flash memory

  *         1: Error occurred while writing data in Flash memory

  *         2: Written Data in flash memory is different from expected one

  */

uint32_t FLASH_If_Write(uint32_t FlashAddress, uint32_t* Data ,uint32_t DataLength)

{

  uint32_t i = 0;

  for (i = 0; (i < DataLength) && (FlashAddress <= (USER_FLASH_END_ADDRESS-4)); i++)

  {

    /* Device voltage range supposed to be [2.7V to 3.6V], the operation will

       be done by word */

    if (HAL_FLASH_Program(TYPEPROGRAM_WORD, FlashAddress, *(uint32_t*)(Data+i)) == HAL_OK)  

//<<<<<<<<<This line returns a HAL_ERROR

    {

     /* Check the written value */

      if (*(uint32_t*)FlashAddress != *(uint32_t*)(Data+i))

      {

        /* Flash content doesn't match SRAM content */

        return(FLASHIF_WRITINGCTRL_ERROR);

      }

      /* Increment FLASH destination address */

      FlashAddress += 4;

    }

    else

    {

      /* Error occurred while writing data in Flash memory */

      return (FLASHIF_WRITING_ERROR);

    }

  }

  return (FLASHIF_OK);

}
    This topic has been closed for replies.

    2 replies

    Tilen MAJERLE
    ST Employee
    May 23, 2018
    Posted on May 23, 2018 at 13:58

    Dear

    hadez803

    ‌,

    what exactly is the issue with IAP?

    Please note that sector_0 address is from0x08000000 to0x08003FFF.

    Best regards,

    Tilen

    harry anders
    Associate III
    May 23, 2018
    Posted on May 23, 2018 at 14:09

    Dear

    Majerle.Tilen

    ,

    I accidentally submitted the question before completing it. I have edited the Question and also fixed the typo about the address of sector_0.

    Best Regards