IAP and External flash
I have 2 questions -
Q1:
Can IAP be used to update the internal flash from an external flash. Here is what I want to do:
1) Download code to the External flash from a remote location. Such as Wifi OTA
2) Have code running looking for new image in the the external flash, notify the user to update by pressing a
a button or two and then have the IAP program the internal flash with the new image.
Q2:
When performing IAP do you need twice the flash as your program. For example, if I have a program that is 32k, do I need 64k to do an IAP. Thought being I'm storing the new program in a section of flash and the the IAP copies that code the program flash. OR does it just overwrite the original program with the new one in the same flash location