Skip to main content
Visitor II
January 22, 2025
Question

I3C Private Write STM32H533RE

Anyone familiar with using I3C in HAL? I'm using I3C to talk to an IMU sensor and I got through DAA and can successfully perform private reads (can read from whoami and other registers also tested) but I couldnt get private writes to work.
I followed 9.8 in this doc (\[Introduction to I3C for STM32 MCUs - Application note\](https://www.st.com/resource/en/application\_note/an5879-introduction-to-i3c-for-stm32h5-series-mcu-stmicroelectronics.pdf)) for Private read which works perfectly however we could not implement a working Private write anywhere in the documentation. We found this (https://github.com/STMicroelectronics/STM32CubeH5/blob/main/Projects/NUCLEO-H533RE/Examples/I3C/I3C\_Sensor\_Private\_Command\_IT/Src/main.c#L79) example code and implemented my own function which doesn’t work. I've been debugging for a week now but still no progress :( Thanks in advance.

 

#define I3C_IDX_FRAME_TX 0U
#define I3C_IDX_FRAME_RX 1U

I3C_XferTypeDef aContextBufs[2]; // Context buffer related to Frame context, contain different buffer value for a communication

uint8_t aTxBuf[15];
uint8_t aRxBuf[31];
uint32_t aControlBuf[0x1F];
I3C_PrivateTypeDef aPrivateDescs[2] =
{
{TARGET1_DYN_ADDR, {aTxBuf, 1}, {NULL, 0}, HAL_I3C_DIRECTION_WRITE},
{TARGET1_DYN_ADDR, {NULL, 0}, {aRxBuf, 1}, HAL_I3C_DIRECTION_READ}};


// callbacks omitted .....

//
int si_io_imu_write_reg(uint8_t reg, const uint8_t *buf, uint32_t len)
{
aTxBuf[0] = reg;
memcpy(&aTxBuf[1], buf, len);

aPrivateDescs[I3C_IDX_FRAME_TX].TxBuf.pBuffer = aTxBuf;
aPrivateDescs[I3C_IDX_FRAME_TX].TxBuf.Size = len + 1;

aContextBufs[I3C_IDX_FRAME_TX].CtrlBuf.pBuffer = aControlBuf;
aContextBufs[I3C_IDX_FRAME_TX].CtrlBuf.Size = 1;
aContextBufs[I3C_IDX_FRAME_TX].TxBuf.pBuffer = aTxBuf;
aContextBufs[I3C_IDX_FRAME_TX].TxBuf.Size = len + 1; // length of the register address + data

// Reset the complete flag
tx_complete_flag = 0;

while (HAL_I3C_GetState(&hi3c1) != HAL_I3C_STATE_READY) {}

if (HAL_I3C_AddDescToFrame(&hi3c1, NULL, &aPrivateDescs[I3C_IDX_FRAME_TX], &aContextBufs[I3C_IDX_FRAME_TX], 1, I3C_PRIVATE_WITH_ARB_STOP) != HAL_OK)
{
return -1;
}

if (HAL_I3C_Ctrl_Transmit_IT(&hi3c1, &aContextBufs[I3C_IDX_FRAME_TX]) != HAL_OK)
{
return -1;
}

while (HAL_I3C_GetState(&hi3c1) != HAL_I3C_STATE_READY)
{
PrintI3CState(&hi3c1);
HAL_Delay(100);
}

// Wait for the transmission to complete
while (tx_complete_flag == 0) {}; tx_complete_flag = 0;

return 0;
}

 

This topic has been closed for replies.

1 reply

Foued_KH
ST Employee
February 10, 2025

Hello @bobycx ,

Could you please check the SDA and SCL signals using oscillator or analyzer .
Which data do you want to send ? 
Which error did you get ? 

Let me know!
Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.