Skip to main content
Associate III
October 11, 2023
Question

I2S Peripheral - Disable slot swapping?

  • October 11, 2023
  • 2 replies
  • 927 views

Hello,

Is there a way to disable the slot swapping of the I2S peripheral?

Take the following example, without any HAL_I2S callbacks...

 

void start_loopback(I2S_HandleTypeDef* is2_handle) {
	printf("--> Starting algorithm loop back...\n");

	for (int i=0; i<I2S_FRAME_SAMPLES; i++){
		i2sTxBuffer[i] = i;
	}

	int hal_res = HAL_I2SEx_TransmitReceive_DMA(is2_handle, i2sTxBuffer, i2sRxBuffer, I2S_FRAME_SAMPLES);
	if(hal_res != HAL_OK) {printf("I2S - HAL_I2SEx_TransmitReceive failed, hal_res = %d!\r\n", hal_res); HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0);}

	while(1){
		vTaskDelay(100);
	}

 

 It unexpectedly produces the following on the receiving end:

 

1 0 3 2 5 4 7 6 9 8 11 10 13 12 15 14 17 16 19 18 21 20 23 22 25 24 27 26 29 28 31 30 

 

 

As I'm consuming and producing I2S samples in software, there is no need for the swap, the DMA buffer will already be in an appropriate format to send over the I2S wire.

This topic has been closed for replies.

2 replies

LCE
Principal II
October 11, 2023

That looks like some DMA buffer / width mismatch.

Start simple, set all to WORD / 32 bit.

Associate III
October 11, 2023

So this ended up being on the receiver side of things, the ESP32:

https://www.esp32.com/viewtopic.php?t=11023

Thanks!