Skip to main content
Associate II
September 27, 2024
Question

I2S-DAC - STM32NUCLEO - F410RB

Is there any example code for I2S to DAC using DMA for generating audios. Will it suitable to generate using wav data or pcm samples to generate audio using this method in this specific controller.

This topic has been closed for replies.

2 replies

AScha.3
Super User
September 27, 2024

>example code for I2S to DAC using DMA for generating audios.

...i dont know. But its only few lines to write - need example for this ?

If using Cube/HAL , the setup DMA -> I2S is done , then only start the dma -- thats all.

here on F411 :

fresult = HAL_I2S_Transmit_DMA(&hi2s5, (uint16_t *) playbuf , (sizeof(playbuf))/2);	// DAC play-loop start

 

>Will it suitable to generate using wav data or pcm samples to generate audio using this method in this specific controller.

I made audio player even with F401 - so : yes, no problem.

If you feel a post has answered your question, please click on " Best Answer ".
AMS12345Author
Associate II
September 27, 2024

@AScha.3 i think the above line help me. but is there possible to get example code? actually i need in nucleof410rb controller.