Skip to main content
khaber9
Associate
January 18, 2009
Question

i2c1 & FSMC

  • January 18, 2009
  • 2 replies
  • 734 views
Posted on January 18, 2009 at 10:50

i2c1 & FSMC

    This topic has been closed for replies.

    2 replies

    khaber9
    khaber9Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Hi,

    I have seen jki has the same problem and have solve it. May be I do something wrong, but I2C1 does not run. Please help.

    I am using I2C1 and FSMC on a STM32F103VC. On the PB6 and PB7 and after RCC_AHBPeriphClockCmd(RCC_AHBPeriph_FSMC, DISABLE), I2C1 works well. After RCC_AHBPeriphClockCmd(RCC_AHBPeriph_FSMC , ENABLE) and remap I2C1 to PB8 & PB9 I2C1 does not work.

    I do following:

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |

    RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD |

    RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO |

    RCC_APB2Periph_USART1, ENABLE);

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2 | RCC_APB1Periph_I2C1 | RCC_APB1Periph_PWR |

    RCC_APB1Periph_SPI2 | RCC_APB1Periph_BKP |

    RCC_APB1Periph_TIM2 |RCC_APB1Periph_DAC, ENABLE);

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_FSMC | RCC_AHBPeriph_DMA1, ENABLE);

    ……….

    #define GPIO_PIN_I2C1SCL GPIO_Pin_8

    #define GPIO_PIN_I2C1SDA GPIO_Pin_9

    GPIO_PinRemapConfig(GPIO_Remap_I2C1, ENABLE);

    // Configure GPIOB Pin8 (SCL) & Pin9 (SDA) as I2C1

    GPIO_InitStructure.GPIO_Pin = GPIO_PIN_I2C1SCL | GPIO_PIN_I2C1SDA;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD;

    GPIO_Init(GPIO_I2C1, &GPIO_InitStructure);

    …….

    Regards

    Klaus Haber

    khaber9
    khaber9Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Hi,

    I found out following: The I2C1 runs on PB8 & PB9 when I also connect pull up resistors on PB6 & PB7. Have anybody an idea what it the reason for this reaction?

    Thanks, regards

    Klaus Haber