Skip to main content
Matthieu Tanguay
Associate II
Jul 20, 2017 8:52 PM UTC
Solved

I2C Troubleshooting without an oscilloscope

Posted on July 20, 2017 at 22:52

Hello everyone,

I recently got myself a little nucleo compatible

http://www.waveshare.com/w/upload/3/3a/Accessory-Shield-Schematic.pdf

that comes with at I2C Temperature sensor 

http://www.nxp.com/docs/en/data-sheet/LM75B.pdf

. After carefully reading the datasheet I felt confident that I could get a working code quick enough. As a first test I decided to try to do a read of the temperature sensor using the pointer. I found some example online that I modified for my needs that look something like that : 

I2C_HandleTypeDef hi2c1;

volatile uint8_t buffer[5];

volatile uint16_t rawTemp;

int16_t Temp;

void TempMeasurement(void){

buffer[0] = 0x00; //Pointer to the Temp. Register

HAL_I2C_Master_Transmit(&hi2c1,0x48<<1,buffer,1,100); //Send pointer for Temperature Register

HAL_Delay(10);

HAL_I2C_Master_Receive(&hi2c1,0x48<<1,buffer,2,100);

//Buffer[0] : MSB

//Buffer[1] : LSB

printf('Buffer After %d\r\n',buffer[0]);

rawTemp = buffer[0]<<5 | buffer[1]; //combine 2 MSB and LSB in one 10 bit number

}

I use the cube to generate the basic code for the I2C Bus. I also know that the sensor is working because I ran the provided mbed code as a check to verify that the electric part of the 'project' is working. If you could help with the code that would be great. On the other hand what I am interested in is ways that I can use HAL librairies to inspect where and how the code is breaking?

I tried to dig into the code and found various values like TIMEOUT and ERROR. Could I use these to check how my bus is failing?

Thank you in advance. 

    This topic has been closed for replies.
    john doe
    john doeBest answer
    Senior III
    Jul 21, 2017 1:09 AM UTC
    Posted on July 21, 2017 at 03:09

    one command looks more complex than the three you're doing? i'm simply adding sanity checks anyone should be doing. making sure the bus is ready. making sure the device is ready.  otherwise, i've actually replaced two commands and a delay, with one. and done some error checking.

    regardless, the point im trying to make is look at the definition of the function you're trying to use and meet it's demands.  the HAL wants a pointer to a buffer's address. you're not giving it that. that may be one of your problems with your code.

    your code:

    HAL_I2C_Master_Transmit(&hi2c1,0x48<<1,buffer,1,100); //Send pointer for Temperature Register

    HAL_Delay(10);

    HAL_I2C_Master_Receive(&hi2c1,0x48<<1,buffer,2,100);

    this is the definition for Master_Transmit

    HAL_StatusTypeDef HAL_I2C_Master_Transmit(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t Timeout)

    it returns the status of the command

    it wants a pointer to the address of the handle

    it wants the device's i2c address, as a 16 bit integer left-aligned

    it wants a pointer to the address of the variable containing the data

    it wants the size of the data in numbers of bytes

    it wants to know how long to wait in ms before the timeout

    your code:

    attempt to transmit

    wait for 10 ms

    attempt to receive

    try:

    is device ready

    if yes, transmit to device

    if no, handle it

    is transmit finished

    if yes, receive response

    if no, handle it

    4 replies

    Vangelis Fortounas
    Associate II
    Jul 20, 2017 10:04 PM UTC
    Posted on July 21, 2017 at 00:04

    Hello!

    In your code   you use  hi2c1 without initialize it

    Is it an external handle initialised somewere else?

    extern I2C_HandleTypeDef hi2c1;

    john doe
    Senior III
    Jul 20, 2017 11:17 PM UTC
    Posted on July 21, 2017 at 01:17

    to read a register use I2C_MemRead();

    while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY) {}

    while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x48<<1), 3, 100) != HAL_OK) {}

    HAL_StatusTypeDef status = HAL_OK;

    status = HAL_I2C_Mem_Read(&hi2c1,                             // i2c handle

                                 (uint16_t)(0x48<<1),                             // i2c address, left aligned

                                 (uint16_t)register_addr,                        // register address

                                 I2C_MEMADD_SIZE_8BIT,                  // device uses 8-bit register addresses

                                 (uint8_t*)(&buffer),                                // variable to put returned value

                                 2,                                                         // return two bytes

                                 100);                                                    // timeout in ms

        if(status != HAL_OK)

        {

          switch(status)

               {

                         case HAL_ERROR: do error stuff; break;

                         case HAL_BUSY: do busy stuff; break;

                         case HAL_TIMEOUT: do timeout stuff; break;

               }

        }

    as far as troubleshooting without a scope goes, you probably have a debugger in your tool chain, and a person can go pretty far with an LED and a few printf() statements

    Matthieu Tanguay
    Associate II
    Jul 21, 2017 2:45 AM UTC
    Posted on July 21, 2017 at 02:45

    Is there an issue doing a receive the way I chose to? Because the 

    I2C_MemRead(); method looks a lot more complex and less straight forward?

    john doe
    john doeBest answer
    Senior III
    Jul 21, 2017 1:09 AM UTC
    Posted on July 21, 2017 at 03:09

    one command looks more complex than the three you're doing? i'm simply adding sanity checks anyone should be doing. making sure the bus is ready. making sure the device is ready.  otherwise, i've actually replaced two commands and a delay, with one. and done some error checking.

    regardless, the point im trying to make is look at the definition of the function you're trying to use and meet it's demands.  the HAL wants a pointer to a buffer's address. you're not giving it that. that may be one of your problems with your code.

    your code:

    HAL_I2C_Master_Transmit(&hi2c1,0x48<<1,buffer,1,100); //Send pointer for Temperature Register

    HAL_Delay(10);

    HAL_I2C_Master_Receive(&hi2c1,0x48<<1,buffer,2,100);

    this is the definition for Master_Transmit

    HAL_StatusTypeDef HAL_I2C_Master_Transmit(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t Timeout)

    it returns the status of the command

    it wants a pointer to the address of the handle

    it wants the device's i2c address, as a 16 bit integer left-aligned

    it wants a pointer to the address of the variable containing the data

    it wants the size of the data in numbers of bytes

    it wants to know how long to wait in ms before the timeout

    your code:

    attempt to transmit

    wait for 10 ms

    attempt to receive

    try:

    is device ready

    if yes, transmit to device

    if no, handle it

    is transmit finished

    if yes, receive response

    if no, handle it