Skip to main content
marcel239955
Associate
Aug 12, 2010 4:36 PM UTC
Question

I2C send only address bytes

Posted on August 12, 2010 at 18:36

I2C send only address bytes

    This topic has been closed for replies.

    4 replies

    marcel239955
    Associate
    May 17, 2011 12:02 PM UTC
    Posted on May 17, 2011 at 14:02

    The ST32 communicate with the component PCA9633 (it is a LED driver)

    I have my code very simplified to find the root cause:

    void I2CInit(void) {

     RCC->APB1ENR |= 0x00400000;      // Pheripherie Clk für I2C1

     RCC->APB2ENR |= 0x00000008;      // Pheripherie Clock für PortB freischalten

     I2C2->CR1 |= 0x8000;       // SWRST

     I2C2->CR1 &= ~0x8000;       // SWRST

     I2C2->CR1 |= 0x0001;       // I/O Pins für I2C einschalten (PE)

     I2C2->CR2 |= 0x00000024;      // FREQ = 36MHz

     I2C2->CCR |= 0x000000B4;      // Busfrequenz = 100kHz

     I2C2->CR1 |= 0x0400;       // ACK

    }

    -------------------------------------------------------------------------------------

    int main (void)  {

    // Slave component: PCA9633

    // PB10 = SCL

    // PB11 = SDA

    I2CInit();

    stm32_Init ();                                  /* STM32 setup */

     for (counter = 0; counter <=255; counter++) {

      I2C2->CR1 |= 0x0100;      // I2C Send I2C start

      delay(50000);

      delay(50000);

        

      I2C2->DR = 0x02;       // PCA9633 slave address

        temp = I2C2->SR1;        // Read SR register to clear ADDR

      temp += temp;

        temp = I2C2->SR2;          // Read SR register to clear ADDR

      temp += temp;

      delay(50000);

      delay(50000);

      I2C2->DR = 0x03;       // PCA9633 control register

      delay(50000);

      delay(50000);

      I2C2->DR = counter;       // Brightness control LED0 Register

      delay(50000);

      delay(50000);

     

      I2C2->CR1 |= 0x0200;      // I2C send stop

      delay(50000);

      delay(50000);

      } 

    }
    Tesla DeLorean
    Guru
    May 17, 2011 12:02 PM UTC
    Posted on May 17, 2011 at 14:02

    >>What do I wrong? Is there a bug?

    Probably a bug in your code, the I2C buses work fine. Try providing some code examples and the chip you are communicating with.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    drzile86
    Associate II
    May 17, 2011 12:02 PM UTC
    Posted on May 17, 2011 at 14:02

    Hi,

    I wrote several codes using I2C bus and I2C bus works just fine. Try to use Standardd Peripheral Examples which you can download on st.com.

    Cheers,

    Dragan

    mtaallah
    Associate
    May 17, 2011 12:02 PM UTC
    Posted on May 17, 2011 at 14:02

    Hi born,

    I have some proposal :

    - Are you sure that GPIO are correctly configured ( AF Open drain).

    - When communication crashs, check if flag errors(ARLO,OVR,AF,BERR) are set or no.

    - Change delay by waiting until TXE flag is set ( after sending one byte wait until TXE flag is equal to 1 after that send the next byte).

    I have some recommendation while using I2C IP : you should after each operation check if related flag are set or no to correctly manage the communication.

    Good Bye.