Skip to main content
larsahl
Associate II
July 9, 2008
Question

I2C read from memory problem

  • July 9, 2008
  • 4 replies
  • 1198 views
Posted on July 09, 2008 at 13:51

I2C read from memory problem

    This topic has been closed for replies.

    4 replies

    larsahl
    larsahlAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:25

    Hello I dont get my code to work for reading from the M24 series memory. I got a 64kb version.

    This is my write code and I think its working but I dont know, becuse I cant read from the memory to verify that.

    void I2C_EE_ByteWrite(u8* pBuffer, u8 WriteAddr)

    {

    /* Send STRAT condition */

    I2C_GenerateSTART(I2C1, ENABLE);

    /* Test on EV5 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));

    /* Send EEPROM address for write */

    I2C_Send7bitAddress(I2C1, EEPROM_ADDRESS, I2C_Direction_Transmitter);

    /* Test on EV6 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

    // send adress 2 times manual says so

    /* Send the EEPROM's internal address to write to */

    I2C_SendData(I2C1, WriteAddr);

    /* Test on EV8 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    /* Send the EEPROM's internal address to write to */

    I2C_SendData(I2C1, WriteAddr);

    /* Test on EV8 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    /* Send the byte to be written */

    I2C_SendData(I2C1, *pBuffer);

    /* Test on EV8 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    /* Send STOP condition */

    I2C_GenerateSTOP(I2C1, ENABLE);

    }

    For reading from the memory I dont really have a clue, but this is my code

    and it doesnt work. Trying to read 1 byte, I want to read more bytes later but im trying just to read one byte right now.

    /* ByteRead code */

    void I2C_EE_ByteRead(u8* pBuffer, u8 ReadAddr)

    {

    // Check busy flag (dont know if I need that but just in case maybe)

    I2C_CheckEvent(I2C1, I2C_FLAG_BUSY);

    // Start

    I2C_GenerateSTART(I2C1, ENABLE);

    // Test EV5

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));

    // Send device adress should it be A0 here or A1? I have no cables to the

    chip enable E0,E1,E2 ports.

    I2C_Send7bitAddress(I2C1, 0xA0, I2C_Direction_Transmitter);

    // Test EV6

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

    // Clear EV6 by setting again the PE bit

    I2C_Cmd(I2C1, ENABLE);

    // Send address for reading

    I2C_SendData(I2C1, 0x1);

    // Test EV8

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    // Send address for reading

    I2C_SendData(I2C1, 0x1);

    // Test EV8

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    // Start

    I2C_GenerateSTART(I2C1, ENABLE);

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));

    I2C_Send7bitAddress(I2C1, 0xA1, I2C_Direction_Receiver);

    // Inactive ACK

    I2C_AcknowledgeConfig(I2C1, DISABLE);

    // I doesnt go in there, what should I do here?

    if(I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED))

    {

    *pBuffer = I2C_ReceiveData(I2C1);

    }

    // Stop

    I2C_GenerateSTOP(I2C1, ENABLE);

    I2C_AcknowledgeConfig(I2C1, DISABLE);

    }

    Please help me im getting gray hair on this one :-[

    morphiq
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:25

    Can u post corrected code?

    larsahl
    larsahlAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:25

    hello ppl!

    Now it works fine, I found some errors in the code ;)

    alexcarrillo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:25

    Quote:

    On 26-02-2008 at 16:57, larsahl wrote:

    // send adress 2 times manual says so

    /* Send the EEPROM's internal address to write to */

    I2C_SendData(I2C1, WriteAddr);

    /* Test on EV8 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    /* Send the EEPROM's internal address to write to */

    I2C_SendData(I2C1, WriteAddr);

    /* Test on EV8 and clear it */

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    Where in the manual it said that you have to sennd the address twice???