Skip to main content
juraj
Associate III
May 7, 2008
Question

I2C master transmitting STOP

  • May 7, 2008
  • 2 replies
  • 661 views
Posted on May 07, 2008 at 03:07

I2C master transmitting STOP

    This topic has been closed for replies.

    2 replies

    kurt2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    I've turned off interrupts just before issuing the STOP command. This seems to work; to start another transfer, you have to turn on interrupts and issue a START command.

    Cheers --Kurt

    juraj
    jurajAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:34

    How should I finish I2C master transmitting? I use this interrupt routine:

    Code:

    void I2C1_EV_IRQHandler(void)

    {

    u32 le=I2C_GetLastEvent(I2C1);

    switch (le)

    {

    /* Test on I2C1 EV5 and clear it */

    case I2C_EVENT_MASTER_MODE_SELECT:

    /* Send I2C1 slave Address for write */

    I2C_Send7bitAddress(I2C1, I2C2_SLAVE_ADDRESS7, I2C_Direction_Transmitter);

    break;

    /* Test on I2C1 EV6 and first EV8 and clear them */

    case I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED:

    /* Send the first data */

    Tx_Idx--;

    I2C_SendData(I2C1, *I2C1_Buffer_Tx++); //EV8 just after EV6

    break;

    /* Test on I2C1 EV8 and clear it */

    case I2C_EVENT_MASTER_BYTE_TRANSMITTED:

    if(Tx_Idx)

    {

    /* Transmit buffer data */

    Tx_Idx--;

    I2C_SendData(I2C1, *I2C1_Buffer_Tx++);

    }

    else

    {

    I2C_GenerateSTOP(I2C1, ENABLE);

    }

    break;

    default:

    break;

    }

    }

    However, I receive next interrupt after

    Code:

    I2C_GenerateSTOP(I2C1, ENABLE);

    How should I regullary stop transmitting? I want to stay in master mode, because after packet is transmitted, next packet should continue.