Skip to main content
evert2
Associate III
November 5, 2013
Question

i2c is not working for stm32f051

  • November 5, 2013
  • 1 reply
  • 716 views
Posted on November 05, 2013 at 16:51

Hello everybody,

I have an application for the STM32f051 wich has a i2c device connected

I have configured and initialized the i2c, however when I send some data both SDA and SDI lines are staying 'high', I don't see any pulses on any of the lines.

I have configured the bus like this:

    /* Connect PXx to I2C_SCL */

    GPIO_PinAFConfig(GPIOB, GPIO_Pin_6, GPIO_AF_1);

    /* Connect PXx to I2C_SDA */

    GPIO_PinAFConfig(GPIOB, GPIO_Pin_7, GPIO_AF_1);

    /*!< Configure I2C pins: SCL */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

    GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_NOPULL;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    /*!< Configure I2C pins: SDA */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

    GPIO_Init(GPIOB, &GPIO_InitStructure);

I have initialized my clocks like this:

         RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA |

         RCC_AHBPeriph_GPIOB |

         RCC_AHBPeriph_GPIOC |

         RCC_AHBPeriph_GPIOF , ENABLE);

         RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM2  |        /* for 1ms timer */

         RCC_APB1Periph_TIM3  |

         RCC_APB1Periph_USART2 |

         RCC_APB1Periph_I2C1 , ENABLE); /* for event timer */

        /* Configure the I2C clock source. The clock is derived from the HSI */

         RCC_I2CCLKConfig(RCC_I2C1CLK_HSI);

I have initialized the i2c bus like this:

   

    /* I2C configuration */

    I2C_InitTypeDef  I2C_InitStructure;

    I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; 

    //I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

    I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable;

    I2C_InitStructure.I2C_DigitalFilter = 0x00;

    I2C_InitStructure.I2C_OwnAddress1 = 0x00;

    I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

    I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

    I2C_InitStructure.I2C_Timing = 0x1045061D; //I2C_TIMING;

    /* Apply I2C configuration after enabling it */

    I2C_Init(I2C1, &I2C_InitStructure);

    /* I2C Peripheral Enable */

    I2C_Cmd(I2C1, ENABLE);

Can anyone say what i'am doing wrong?

Thanks in advance,

Evert

#stm32f051-i2c-init
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
November 5, 2013
Posted on November 05, 2013 at 16:59

PinAFConfig needs PinSource (index) not Pin (mask) values.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..