Question
I2C Communication Flow (Brain Storming)
Posted on August 10, 2016 at 16:04
All,
For the basic I2C program flow I want to send the start condition, send the address, send the data and then generate the stop condition. You can see below that after each action I am polling for a flag to move one to the next stage.My goal is to send an entire I2C transaction of start, address, data, stop and then repeat this over and over so I can look carefully at my scope.Note: I am working on a dev board that doesn't have my I2C slave device on it. I am trying to just see the basic communication out on my scope but I won't be hearing back from the slave device. This is why on the Send7bitAddress I am checking to see if there was no ACK because there won't be and I know the address should have been sent out. Just to give the full context I want to get the below code to send out a ''full transaction'' without the chip I am using on the board for some initial testing.1.) Does the flow below make sense? It looks like I need one more section of sending out the data (register plus the data).2.) I was not sure what flag to check after sending the address because this will not impact TxE. Do the flags that I am checking for make sense?Thank you for any additional thoughts on this. I2C3_Init(); while(1) { I2C_GenerateSTART(I2C3, ENABLE); while( I2C_GetFlagStatus(I2C3,I2C_FLAG_SB) == RESET ); I2C_Send7bitAddress(I2C3, 0x21, I2C_Direction_Transmitter); // SEND ADDRESS while( I2C_GetFlagStatus(I2C3,I2C_FLAG_AF) == RESET ); I2C_SendData(I2C3,0xAA); while( I2C_GetFlagStatus(I2C3,I2C_FLAG_TXE) == RESET); I2C_GenerateSTOP(I2C3, ENABLE);while( I2C_GetFlagStatus(I2C3,I2C_FLAG_STOPF) == RESET );
}-Mike