I2C code on STM32Cube_FW_L0_V1.10.0
Hi,
Today I upgraded the firmware packages in STM32CubeMX and was looking at the differences with the version I had previously installed (v1.8.1 in the source files) and noticed the following definitions in stm32l0xx_hal_i2c.h:
#define I2C_NO_STARTSTOP (0x00000000U)
#define I2C_GENERATE_STOP (uint32_t)(0x80000000U | I2C_CR2_STOP)#define I2C_GENERATE_START_READ (uint32_t)(0x80000000U | I2C_CR2_START | I2C_CR2_RD_WRN)#define I2C_GENERATE_START_WRITE (uint32_t)(0x80000000U | I2C_CR2_START)and the following code on stm32l0xx_hal_i2c.c, function I2C_TransferConfig:
MODIFY_REG(hi2c->Instance->CR2, ((I2C_CR2_SADD | I2C_CR2_NBYTES | I2C_CR2_RELOAD | I2C_CR2_AUTOEND | (I2C_CR2_RD_WRN & (uint32_t)(Request >> (31U - I2C_CR2_RD_WRN_Pos))) | I2C_CR2_START | I2C_CR2_STOP)), \
(uint32_t)(((uint32_t)DevAddress & I2C_CR2_SADD) | (((uint32_t)Size << I2C_CR2_NBYTES_Pos) & I2C_CR2_NBYTES) | (uint32_t)Mode | (uint32_t)Request));I would like to know why the I2C_GENERATE_* definitions are ORed with 0x80000000?, in the datasheet I'm looking (stm32l051) the msb is defined as reserved, also, the second argument in the macro MODIFY_REG includes this:
(I2C_CR2_RD_WRN & (uint32_t)(Request >> (31U - I2C_CR2_RD_WRN_Pos)))
and it doesn't make much sense, is there something I am missing?