Skip to main content
DiBosco
Senior
July 15, 2010
Question

I2C clock stretching in master mode and other I2C issues

  • July 15, 2010
  • 3 replies
  • 789 views
Posted on July 15, 2010 at 17:13

I2C clock stretching in master mode and other I2C issues

    This topic has been closed for replies.

    3 replies

    greg_t
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:58

    Hello,

    Clock streching is used by slow slaves .. If your slave perform some calculations or other tasks with the recieved data on I2C it holds the clock low until finished proccesing the data (may be interrupt routine ). After releasing the clock the Master may send another byte of data .....

    DiBosco
    DiBoscoAuthor
    Senior
    May 17, 2011
    Posted on May 17, 2011 at 13:58

    @Gregory, thanks for the clarification.

    @Crossware, thanks for that, I shall implement that for if/when it gets stuck.

    I found an error on the layout of the Atmel chip which seems to have helped a lot as well.

    stforum2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:58

    We found it necessary to reset the I2C (in order to clear the busy bit if I recall):

        g_pRCC->APB1ENR |= I2C1EN;

        g_pI2C1->CR1 = I2C_SWRST;

        g_pI2C1->CR1 = 0;

        g_pI2C1->CCR = I2C_CCR7 | I2C_CCR5;

        g_pI2C1->TRISE = 0X09;

        g_pI2C1->CR2 = I2C_FREQ5;

        g_pI2C1->CR1 = I2C_PE;