I would like to know if there is a way to setup IPCC in Cube MX 6.3
In UM1718, it states that IPCC is only used for the STM32MP1 series.
I understand that I need to update the version that I'm using however, I do not want to loose and have to restart again for our project.
Furthermore, I've tried to use the H747 and other dual core MCU's but, only the series MP1 indicates the IPCC.
I need to communicate and share data from CM7-CM4 and visa versa.
- is there a way to setup IPCC in Cube MX 6.3 or do I need to use STM32 Cube H?
If I can use the current version I have, how do I establish a communication link between cores in Cube MX? Please recommend the documentation that I would need.
AHB, Simplex Communication I've studied but, I have not solidified the setup.
Thanks,
Hiram