Skip to main content
VP_it
Associate
July 17, 2020
Question

I would like to know ,how to program STM32F103RCT6 microcontroller using Cyclone univeral programmer?

  • July 17, 2020
  • 2 replies
  • 1353 views

I have connected in port B(SWD Interface), i tried both powering modes with no jumpers and with 1,2,3 jumper.

i am getting a error note $00000007 cannot enter into debug mode.

what may be the issue.?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
July 17, 2020

Not really a Cyclone support site here, definitely don't see much traffic. Talk to PE Micro's support.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SMcGr
Associate II
August 24, 2020

Hello,

Generally and error $00000007 using the Cyclone Universal means that communication cannot be established with the target either due connection issue, power settings, or a setting that was used to establish communication. I would check that the ribbon cable is oriented correctly first. Then there should be an icon in the top right of the Cyclone LCD screen indicating whether the target is currently powered or not. If everything seems to be oriented correctly and the target has power, there may be an issue when selecting the programming algorithm or another setting before attempting to connect.

If you are able to provide some details on your connection setup, then we could go further.

Steve