Question
I wonder if it is possible to use the DAC in STM32G4 to produce a 30kHz sinewave with 1Hz resolution.
The application is to fine tune acoustic resonantors. In other words we want to be able to tune DMA DAC output from 29.990 to 30.010 in 1 Hz steps. Ideally we also would like to tune the amplitude. There are some ideas with DAC reference prescalers and different LUTs. Any idea for a more elegant solution?