Skip to main content
CJone.1
Associate
June 2, 2020
Question

I wish to use the 48-pin version of the L5. If I buy a L5 Nucleo board can I target a 48-pin device and debug the code for the 48-pin device on the Nucleo board even though it has a 144-pin part fitted.

  • June 2, 2020
  • 5 replies
  • 1046 views

..

This topic has been closed for replies.

5 replies

waclawek.jan
Super User
June 2, 2020

You did not tell us which 'L5 exactly, but luckily this is a small family and it's basically the same silicon die in all models.

If the Nucleo has all pins you need brought out, then yes, you can use it.

JW

CJone.1
CJone.1Author
Associate
June 2, 2020

​Hi JW,

Thank you for the speedy reply. So if I build an image for a STM32L562CE I will be able to flash it into the L5 Nucleo board?

Obviously only the pins I have configured in the STM32L562CE will be activated in the 144-pin L5 on the Nucleo board.

Correct?

Regards

Chris

waclawek.jan
Super User
June 2, 2020

If the chip on Nucleo 'L552 or 'L562?

In the former case you won't be able to use the crypto functionality.

Also, I don't know whether the are SMPS variants of the 'L5s (P and Q suffixed part numbers); that might make some difference, too.

Other than that, it should be as you've said above.

JW

CJone.1
CJone.1Author
Associate
June 2, 2020

​Awesome!

Thanks JW, you can close.

Best regards

Chris

ST Technical Moderator
June 2, 2020

Hello,

Yes, it is possible. Just consider using 48-pin IOs.

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks